What is PCB Signal Attenuation: How Signals Weaken Over Distance and How to Mitigate It
10 min
- What is Attenuation? Meaning & Definition
- PCB Substrate Material Selection for Attenuation Control
- Causes of Signal or Cable Attenuation
- Preventing of Improving Attenuation Rate
- How to Calculate Signal Attenuation?
- Why does the Signal Attenuate When it Travels in Wire?
- What Causes Signal Attenuation in PCBs?
- Other Ways to Reduce Signal Attenuation?
- Design Tips for Better Signal Integrity:
- FAQ about PCB Signal Attenuation
- Conclusion:
Key Takeaways
- Primary Causes: Signal attenuation is mainly caused by skin effect (conductor loss) and substrate energy absorption (dielectric loss).
- How to Mitigate: Reduce loss by using wider traces, low-loss materials, controlled impedance, and removing via stubs.
- JLCPCB Solutions: JLCPCB offers Rogers high-frequency laminates, High-TG FR4, precision impedance control, and backdrilling to protect signal integrity.
As a signal travels from the source to the load through PCB conductors, the signal is attenuated due to trace resistance and dielectric losses, resulting in energy loss. Signal attenuation is the most common term used when high-speed signals travel across a circuit board. It is one of the major contributors to signal degradation that leads to signal integrity issues. Usually more attenuation can be seen at higher frequencies due to phenomena like skin effect.
The attenuation factor determines how far a signal can travel and still provide enough data bits or information. It quantifies different transmission media based on how the amplitude of the transmitted signal decreases with frequency. It is given by:
Signal attenuation (α) is quantitatively defined in decibels per unit length (dB/inch or dB/cm). The total attenuation in decibels is calculated using:
Attenuation (dB) = -10 log10 (Pout/Pin) = -20 log10 (Vout/Vin)
Where Pin and Vin represent input power and voltage, and Pout and Vou represent output power and voltage at the load.
What is Attenuation? Meaning & Definition
Attenuation is the reduction in the amplitude of a signal as it travels through a medium. Attenuation can be caused by transmission loss, reflection, or absorption. In an electrical system, attenuation is a decrease in voltage as it flows along a wire or other transmission line. Attenuated systems can also be referred to as degraded systems.
Attenuation is expressed in decibels (dB) and represents the ratio of output to input power or intensity. Attenuation values can range from zero decibels for an unobstructed or perfect transmission, to extremely large negative numbers. A perfect attenuator with 0 dB of attenuation has an infinite number of taps along the transmission line.
PCB Substrate Material Selection for Attenuation Control
While layout optimization is crucial, selecting the appropriate PCB substrate material is the primary decision for controlling dielectric loss at high frequencies. Dielectric absorption increases linearly with signal frequency, making low-loss laminates essential for high-speed designs.
To help designers mitigate signal attenuation, JLCPCB offers a variety of base materials ranging from standard FR-4 to high-frequency RF laminates. The table below compares the key dielectric properties and attenuation characteristics of popular PCB substrates supported by JLCPCB:
| Material / Substrate | Dielectric Constant (Dk @ 1GHz) | Dissipation Factor (Df / Loss Tangent) | Attenuation Performance | Recommended Applications |
|---|---|---|---|---|
| Standard FR-4 (e.g., Nan Ya / ShengYi) | 4.3 - 4.5 | 0.015 - 0.020 | High Loss | Low-speed & General Digital (< 1-2 GHz) |
| High-TG FR-4 (e.g., S1000-2M / IT-180A) | 4.2 - 4.4 | 0.010 - 0.015 | Moderate Loss | High-Density & Mid-Speed Interconnects |
| Rogers RO4350B (JLCPCB RF Option) | 3.48 ± 0.05 | 0.0037 | Very Low Loss | RF, Microwave & High-Speed Data (> 5-10 GHz) |
| Rogers RO4003C | 3.38 ± 0.05 | 0.0027 | Ultra Low Loss |
Causes of Signal or Cable Attenuation
When we talk about signal or cable attenuation, we are talking about signal degradation between a transmitter and receiver. Signal loss can be caused by many variables that affect cable quality, such as:
- Poorly manufactured fiberoptics (bad connectors and poor splices)
- Excessive bending of the cable. This causes signal reflections.
- Operating at higher signal wavelengths.
- Long signal cable runs between transmitter and receiver (attenuation increases over signal cable length).
Preventing of Improving Attenuation Rate
Practical Strategies to Minimize Attenuation in PCB Layout (JLCPCB DFM Best Practices)
Signal attenuation can be mitigated using the following PCB layout and fabrication techniques:
1. Optimize Trace Geometry & Impedance Control: Design wider signal traces where space permits to increase surface area and lower skin effect resistance. Utilize JLCPCB’s Impedance Control Service (±10% or ±5% precision) to ensure consistent 50 Ω single-ended or 100 Ω differential impedance and avoid reflection losses.
2. Select Low-Df Laminates: Upgrade from standard FR-4 to High-TG FR-4 or Rogers RO4350B/RO4003C for lines carrying signals above 3 GHz.
3. Minimize Via Stubs (Backdrilling): Unused via stubs create resonant reflections that severely attenuate specific frequency notches. Specify JLCPCB Backdrilling (Controlled-Depth Drilling) for high-speed vias operating above 6 Gbps.
4. Keep Traces Short and Direct: Avoid unnecessary routing lengths and layer transitions.
How to Calculate Signal Attenuation?
Signal attenuation is estimated in decibels (dB) per unit length of the transmission medium. It can be calculated in terms of power and voltage.
To avoid the chance of fading, multiple signals are sent to ensure that at least one reaches the final destination, the receiver. But due to the need to send these extra signals, this approach slows down the overall network speed. The lower the attenuation, the more efficient the transmission medium is. Higher attenuation means more signal loss and reduced amplitude on the receiver side.
Why does the Signal Attenuate When it Travels in Wire?
The amplitude of the signal is distorted by trace resistance and the dissipation factor of the circuit board dielectric. This effect is more prominent at high frequencies since signals tend to propagate along the trace surface. Attenuation causes slower signal rise times and increases the likelihood of data errors.
Signal attenuation in printed circuit boards consists of three major components:
1. Conductor Loss & Skin Effect (Ac)
At DC and low frequencies, current density is uniform across the trace cross-section. As frequency increases, the self-inductance forces current to concentrate near the outer surface of the conductor (Skin Depth, δ). Skin depth is calculated as:
δ = √(ρ / (π · f · μ))
As skin depth decreases, the effective cross-sectional area shrinks, increasing AC resistance and causing significant signal attenuation at high frequencies.
2. Dielectric Loss (Ad)
The dielectric substrate between the signal trace and reference plane dissipates energy as heat when exposed to alternating electric fields. Dielectric attenuation increases linearly with frequency (f) and is directly proportional to the Loss Tangent (tanδ or Df):
Ad ≈ 2.3 · f · √(εr) · tanδ [dB/inch]
High-frequency PCB designs require materials with ultra-low Df, such as Rogers RO4350B available at JLCPCB.
3. Copper Surface Roughness Loss (Ar)
At high frequencies where skin depth is less than the copper surface profile height (Rz), the signal current is forced to follow the contours of the rough copper profile. This lengthens the effective path and dramatically increases resistive loss. JLCPCB utilizes controlled copper foil profiles (e.g., Very Low Profile - VLP copper) on high-frequency stackups to minimize roughness-induced attenuation.
What Causes Signal Attenuation in PCBs?
As the signal range increases, so does the attenuation. Factors like low trace width
And crosstalk also plays a role in signal attenuation. Some factors listed below are responsible for signal attenuation:
Transmission frequency: The shorter the wavelength, the greater the attenuation of radio waves. Such signals are transmitted via 2.4GHz or 5GHz electromagnetic waves. Electromagnetic waves have high frequencies and short wavelengths. Therefore, radio signals have large attenuation and cannot be transmitted over long distances.
Resistive losses associated with conductor materials: The conductive materials used to manufacture transmission lines, such as copper, introduce resistive losses that cause attenuation of signals traveling on copper traces.
Losses Related to Dielectric Materials: Dielectric losses are introduced by losses in the dielectric material sandwiched between transmission lines. This dielectric loss creates a conductance in the substrate, also known as reverse resistance, and absorbs some of the propagated signal energy, causing signal attenuation.
Copper Surface Roughness: Copper surface roughness on a PCB also acts as a resistance to signal propagation. Rough copper traces increase resistance because the topography of the copper surface moves the signal up and down. Surface spikes also increase capacitance. Smooth copper is a solution to this problem, but is more expensive.
Other Ways to Reduce Signal Attenuation?
Signal attenuation can be mitigated using the following techniques:
Use a repeater: If the received signal is weak, use a repeater to regenerate the original signal by reducing attenuation. It also enhances the range of the signal, allowing it to transmit longer distances without failure.
Use an Amplifier: If the received signal is weak, an amplifier is used to increase its amplitude, unlike a repeater which regenerates the entire signal.
Proper material selection: Careful selection of low-loss dielectric materials and low-resistance traces can minimize signal attenuation.
Use programmable differential output voltage (VOD) settings: Programmable VOD ensures drive strength is synchronized with line impedance and trace length. Increasing VOD at the driver enhances the signal at the receiver.
Pre-emphasis: Using amplifiers to increase signal strength is not the only solution for attenuation control, as it also amplifies the associated signal noise and jitter. Pre-emphasis only enhances the high-frequency components of the signal by increasing the level of the first transmitted symbol. If subsequent symbol levels are transmitted at the same level, they will remain unchanged. For example, if a signal transmits a high level for three symbols, only the first symbol is emphasized. The next two symbols will be transmitted at the usual levels.
Design Tips for Better Signal Integrity:
- Place the antenna closer to the source.
- Improve conductivity by wiring together different materials.
- Make sure that there is nothing interfering with the signal.
- Place antennas far away from any metallic objects.
- Use a power amplifier for stronger signals if needed.
FAQ about PCB Signal Attenuation
Q: What is the primary cause of signal attenuation in high-speed PCBs?
Signal attenuation is mainly caused by conductor loss from the skin effect and dielectric loss from substrate dissipation. At high frequencies, current concentrates on the trace surface, increasing resistance, while the substrate material absorbs signal energy as heat.
Q: How does copper surface roughness affect signal attenuation?
At high frequencies, current flows along a thin surface layer. If the copper surface is rough, current follows the uneven contours, effectively lengthening the trace path and increasing resistance and signal loss. Using low-roughness copper foils reduces this loss.
Q: When should I upgrade from standard FR4 to Rogers laminates?
For high-speed or RF designs operating above 3 to 5 GHz, standard FR4 causes excessive signal loss over long traces. Upgrading to Rogers materials significantly reduces dielectric loss, maintaining signal integrity for sensitive applications.
Q: What is a via stub and how does backdrilling reduce attenuation?
A via stub is an unused portion of a plated through hole. It acts like an open line and creates reflections that attenuate signals at specific frequencies. Backdrilling removes this unused stub to eliminate reflections and improve signal quality.
Q: How does JLCPCB help engineers minimize PCB signal attenuation?
JLCPCB provides precision impedance control, advanced high-frequency substrates like Rogers and High-TG FR4, optimized layer stackups, and backdrilling services to reduce trace losses and reflections.
Conclusion:
Addressing signal attenuation requires a comprehensive approach balancing material properties, trace geometry, and accurate fabrication. By leveraging low Df substrates, controlling impedance, and utilizing advanced manufacturing options like backdrilling, engineers can ensure high-speed signal integrity. JLCPCB provides robust high-frequency manufacturing capabilities—including Rogers laminates, precision impedance control, and advanced stackups—helping designers turn high-speed PCB layouts into high-performance, low-loss hardware.
Popular Articles
Keep Learning
Navigating the Impedance Landscape: Selecting the Right Impedance for USB, Ethernet, HDMI, and SD Card Interfaces
Introduction In the realm of high-speed digital communication, choosing the right impedance is a critical aspect of successful PCB design. Impedance matching ensures optimal signal integrity, minimizes reflections, and enhances the overall performance of interfaces such as USB, Ethernet, HDMI, and SD Card. In this blog post, we'll explore the importance of impedance, the factors influencing impedance selection, and best practices for ensuring reliable data transmission in these widely used interfaces.......
A Beginners Guide to Impedance Control in PCBs
When a digital signal is transmitted from one point to another, it causes a change in the state of the signal line. This change can be understood as an electromagnetic wave moving through the circuit. Reflection occurs when this wave encounters a boundary between different mediums. At this boundary, some of the wave's energy continues as a signal, while the rest is reflected. This process repeats until the energy is either absorbed by the circuit or dissipated into the environment. For electrical engi......
What is PCB Signal Attenuation: How Signals Weaken Over Distance and How to Mitigate It
Key Takeaways Primary Causes: Signal attenuation is mainly caused by skin effect (conductor loss) and substrate energy absorption (dielectric loss). How to Mitigate: Reduce loss by using wider traces, low-loss materials, controlled impedance, and removing via stubs. JLCPCB Solutions: JLCPCB offers Rogers high-frequency laminates, High-TG FR4, precision impedance control, and backdrilling to protect signal integrity. As a signal travels from the source to the load through PCB conductors, the signal is ......
Understanding Analog and Digital Ground in PCB Design
When working on printed circuit board (PCB) design, proper grounding is crucial for ensuring signal integrity, minimizing noise, and maintaining reliable performance. Two common types of ground planes used in PCB layouts are Analog and Digital ground. In this article, we will explore the differences between analog and digital ground, their significance in PCB design, and best practices for their implementation. Analog Ground vs. Digital Ground Analog ground and digital ground have separate purposes in......
Design Guide for USB-3.0 Differential Signaling
In the world of data transfer, USB 3.0 is the Usain Bolt to USB 2.0’s friendly jogger. USB 2.0 is called “High Speed” and limped along at 480 Mb/s, whereas USB 3.0 SuperSpeed rockets up to 5 Gb/s (over ten times faster). But this speed jump brings full‑duplex operation and new differential transmit (SSTX) and receive (SSRX) pairs on dedicated pins. USB 2.0 D+/D– lines handle enumeration and legacy data, while two new 5 Gb/s high‑speed differential pairs carry SuperSpeed data in each direction. While m......
Understanding Impedance Matching for High-Speed PCB Designs
With the advancement of technology and the ever wider application of integrated circuits, the frequency and speed of electronic signal transmission have been increasing, making it essential for PCB conductors to provide high-performance transmission lines. These transmission lines are responsible for delivering signals from a source to the input of a receiver accurately and completely. This requirement emphasizes the need for impedance matching. Electrical impedance, commonly represented as Z and meas......