This website requires JavaScript.
Coupons APP Download
Ship to

Thermal Relief Via Covering

Thermal Relief Via Covering
Thermal Relief Via Covering

85*******4A

2024-11-05 23:48 PM

Hi!


I'd like to add thermal relief vias to a QFN thermal pad, but since epoxy/copper filling is expensive, I want to ask if it is possible to use tented vias instead. To make sure the vias are covered, I left some clearance in the solder resist layer around them (see below).



Also, solder paste covering of the exposed pad surface is around 50% to prevent liftoff of the package during reflow.


Please advise me, is this a good idea? Thanks!