Digital 101: What is a State Machine in Digital Electronics
6 min
- What is a State Machine?
- Why State Machines Matter in Digital Electronics
- Components of a State Machine
- Types of State Machines
- How to Design a State Machine
- Applications of State Machines in Electronics and PCB Design
- Advantages and Limitations of State Machines
- Difference Between Moore and Mealy State Machines
- Conclusion:
People say everything that exists in nature is analog, and digital is just a manmade approach to simplify and make faster computations. Digital systems are used in signal processing to storage devices, because of their small standardized size and low power consumption. Moreover, there are MCUs and FPGAs that can do the computations only in digital format, but there is always an option to reconstruct the signal using DACs and ADCs. Today, we will talk about state machines. These are basically the small units that make a big system. For example, a microcontroller is nothing but a combination of different state machines.
The computation in a state machine digital system is done by analyzing system behaviour differently based on its current conditions (states) and inputs. It is just about moving from one state to another based on some type of input logic or past inputs. Whether you are an electronics student or an engineer, understanding state machines is a skill that pays off across multiple domains.
What is a State Machine?
A state machine is a mathematical model used to describe the behavior of a system based on a finite number of conditions in digital electronics called states. At any given time, a digital system can only be in one state. Now, based on inputs, it transitions to the next state while generating outputs. Using these states and inputs, the next state is decided; that’s how any microcontroller at the register level works. Everything depends on the set of input given by the user. Think of it like a traffic light controller:
- It has states (Red, Yellow, Green).
- It changes states based on timers (inputs).
- Each state dictates the output (which light is ON).
This structured design helps engineers build predictable, reliable, and scalable digital systems.
Why State Machines Matter in Digital Electronics
State machines are vital in sequential logic design, where the output depends not only on the current inputs but also on past behavior (previous states). Unlike combinational logic circuits (where output depends only on inputs), state machines introduce memory elements. They matter because:
- They form the control logic of microprocessors and digital systems.
- They are essential for protocol handling in communication (e.g., UART, I2C, SPI).
- They simplify embedded controllers for automation and industrial electronics.
Components of a State Machine
Every state machine consists of the following building blocks:
- States – The different conditions a system can be in.
- Transitions – Rules for moving from one state to another.
- Inputs – External signals that trigger state changes.
- Outputs – Actions or signals produced in a given state.
- State Register – Typically built with flip-flops to hold the current state.
- Next-State Logic – Determines the next state based on the current state and inputs.
Types of State Machines
There are two major types of finite state machines (FSMs) in digital electronics:
1. Moore State Machine:
The output of the circuit depends only on the current state in this case. The inputs affect the next state, but not the output directly. These machines are somewhat simpler and more predictable.
Example: Elevator controller – The door open/close signal depends only on the current floor (state).
2. Mealy State Machine:
The output depends on the current state + inputs. It has a faster response since inputs can immediately affect the output. More machines are compact but slightly more complex.
Example: Serial data receiver – The output (data bit) depends on both the current receiving state and the incoming signal.
How to Design a State Machine
So basically, it is a machine that can be used to change the state. We can apply any logic to it, from a simpler to a more complex one. Designing a state machine follows a structured approach:
1. Define the Problem
The design of the control system should be clear, like what we are designing and how it actually works. The functionality of the system should be known to the designer. Example: Traffic light sequence.
2. Identify Inputs and Outputs
Then we define the type of inputs and outputs the system has, for example, the traffic light controller has a sensor, button, and clock signal as the inputs and LED signals as the outputs.
3. Create a State Diagram
Then we have to draw the diagram, using the transitions and states, showing how the logic is changing when the inputs and past states are changing. This is defined with the help of a diagram, which makes it easy to understand and create a logical transition table.
4. Build a State Transition Table
It is the tabular representation of states, input, output, and next states. It has all the combinations in which the input is changing and past states are there, so it helps to determine the next state of the system.
5. Implement the Logic
With the help of a transition table, the logic is clear now to implement the logic that the digital elements are used for. In which the flip-flops are used for the state storage, and a combination circuit for the other logic.
Applications of State Machines in Electronics and PCB Design
State machines are widely used in both digital IC design and PCB system-level design. Where the microcontrollers are not necessary, we use the state machine application-specific integrated circuits to cut down the cost and space of the overall system. Some notable applications include:
- Microcontrollers and CPUs: The control unit is essentially a state machine.
- Communication Protocols: UART, I2C, SPI, and CAN bus use FSMs for handshaking and data transfer.
- Robotics and Automation: Used in sequence controllers, robotic arms, and PLC systems.
- Consumer Electronics: Washing machines, microwaves, and other appliances use FSMs for process control.
Advantages and Limitations of State Machines
The state machines have more predictable and relative behaviour, because they implement the small and structured logic, so easier debugging can be done. Moreover, they can be scaled as per application and well well-suited for ASIC/FPGA implementation.
But some logic may explode in size, which makes them very hard to implement. Moore machines can be slower, and Mealy machines can be glitch-prone due to the complexity and input dependency.
Difference Between Moore and Mealy State Machines
Conclusion:
A state machine in digital electronics is a predictable and structured digital system. From simple vending machines to advanced CPU controllers, FSMs are everywhere. These are the most common and widely used building blocks of sequential logic design. We have seen the difference between the two types of machines: Mealy and Moore machines. We have seen the internal logic and the design procedure of machines from simple problem statements to state logic implementation.
For students, learning about Moore and Mealy state machines builds a strong foundation in digital design. For electronics and PCB engineers, FSM knowledge translates directly into designing robust logic blocks.
Popular Articles
• Choosing the Best PCB Color-Enhancing Aesthetics and Functionality
• PCB Silkscreen: All You Need to Know
• The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
• Understanding Electrical Schematics: A Comprehensive Guide
• PCB Board Design: A Step-by-Step Guide for Beginners
Keep Learning
A Beginner's Guide to Basic Electronic Components: Functions, Symbols & Uses
Every circuit, from a simple LED flashlight to a microcontroller board, is built from the same handful of common electronic components. This guide breaks down the ten basic electronic components you will encounter most often: What each component does How it works Key specifications Where engineers use it By the end, you will be able to recognize these electronic circuit components on a schematic, a PCB, or a parts bin, and know exactly why each one is there. These electronic components are the buildin......
Capacitor Voltage Rating Explained with Examples
Capacitors are small components widely used not only for power delivery but also for signal conditioning in electronic circuits. In this article, we focus on the capacitor voltage rating across different types of capacitors. At first glance, capacitors look simple—small cans, discs, or chips on a PCB. However, their markings carry essential design information, including capacitance and voltage rating. These are not arbitrary values but directly affect circuit reliability. Ignoring the voltage rating w......
From Prototype to Product with a Better Development Board
Note Prototype Fast: Development boards integrate power, clock, and programming circuits to validate firmware in hours. Pick the Right Platform: Use ESP32 for Wi-Fi/BLE, Arduino UNO for 5 V sensors, Raspberry Pi Pico for tight I/O timing, and Raspberry Pi 5 for Linux. Scale to Custom PCB: Reuse your prototype's certified module, firmware, and support circuits, but remove unused headers to cut unit cost. Build for Production: Use a 4-layer ground-plane stackup for wireless boards, verify BOM stock earl......
4 Layer vs 6 Layer vs 8 Layer PCB: How to Choose the Right Stackup
Random selection of layers in electronics may lead to serious signal integrity issues. That's why we always design our stackup before designing the PCB. Stackup decides the type of PCB and how it gonna perform under high-frequency conditions. There are a lot of things that directly affect the stackup of the PCB, related to impedance matching, routing density, signal and power integrity, electromagnetic compatibility (EMC), and cost. Knowing the requirements before design and the most critical componen......
Choosing the Best PCB Color-Enhancing Aesthetics and Functionality
Key Takeaways Choosing the best PCB solder mask color involves balancing aesthetics, visibility, and functionality. Green remains the top choice for superior contrast and inspection, while black offers premium appeal, white excels in LED applications, and other colors like purple and red provide unique design options. The ideal color depends on your priorities in inspection ease, thermal performance, and brand image, with minimal impact on electrical performance when using proper silkscreen contrast. ......
Single-Sided PCB Design: Combining Simplicity with Sophistication
Key Takeaways Single-sided PCBs offer a simple, cost-effective solution for many electronic applications. SMT and THT components require different mounting and soldering arrangements. Proper layer orientation, Gerber files, and design rules help ensure manufacturability. Aluminum PCBs require careful attention to insulation, component mounting, and silkscreen placement. A printed circuit board (PCB) provides mechanical support for electronic components and establishes the electrical connections requir......