PCB Basic 3: Understanding PCB Manufacturing Processes
9 min
- Substrate Selection: Laying the Foundation
- Layer Imaging and Etching: Giving Shape to Your Design
- Finishing: Protecting and Enhancing Your PCB
- Advanced Manufacturing Techniques: Pushing the Boundaries
- Quality Control Measures and Inspection Methods
- Conclusion:
Welcome to the third installment of our PCB Basics series. In this article, we will unravel the step-by-step process of PCB manufacturing, guiding you through each stage with clarity and precision.
Join us as we embark on this educational journey and discover how JLCPCB's advanced manufacturing capabilities and technology together with unparalleled commitment to quality assurance can elevate your PCB designs to the next level.
Substrate Selection: Laying the Foundation
One of the critical steps in PCB manufacturing is selecting the right substrate material. The substrate serves as the foundation upon which the circuitry is built. It is essential to choose a substrate material that meets the electrical, thermal, mechanical, and cost requirements of your design. The choice of substrate material can impact the performance, reliability, and manufacturability of the PCB.
FR-4 is the most commonly used substrate material in the industry due to its excellent electrical insulation properties and cost-effectiveness. It is composed of woven fiberglass impregnated with an epoxy resin. The combination of fiberglass and epoxy provides a robust and rigid base for the PCB. JLCPCB uses Grade A FR-4 laminates from suppliers including Nan Ya, KB, and Shengyi, with Tg options of 130°C (standard) or 155°C (high Tg) for enhanced thermal performance. Additionally, FR-4 offers good thermal stability and dimensional stability, making it suitable for a wide range of applications.
Flexible materials, such as polyimide (PI), are ideal for applications that require flexibility or bending. These materials offer excellent resistance to heat and chemicals, making them suitable for aerospace, automotive, and wearable electronics.
Specialized substrates, such as Rogers materials (including Rogers and PTFE/Teflon variants), are designed for high-frequency applications where signal integrity is crucial. These materials have low dielectric loss and can provide consistent performance at high frequencies.
By carefully considering the electrical, thermal, mechanical, and cost requirements of your design, you can select the most suitable substrate material that ensures optimal performance and reliability.
Layer Imaging and Etching: Giving Shape to Your Design
Once the substrate is selected, the next step is layer imaging and etching. Layer imaging involves transferring the PCB design onto the substrate surface. The process begins by applying a thin layer of photosensitive material, called photoresist, onto the substrate. The photoresist is then exposed to UV light through a photomask, which contains the desired PCB pattern. The UV light causes a chemical reaction in the photoresist, creating a patterned layer.
After the layer imaging process, the unwanted copper on the substrate is removed through etching. Etching is achieved by immersing the substrate in an etchant solution that selectively dissolves the exposed copper, leaving behind the desired circuit pattern. The etchant solution typically contains chemicals such as ferric chloride or ammonium persulfate.
To ensure precise and accurate etching, it's important to control the etching time, temperature, and agitation of the etchant solution. Over-etching can result in thin or weak traces, while under-etching can leave excess copper, causing short circuits or signal integrity issues.
Finishing: Protecting and Enhancing Your PCB
Finishing processes play a crucial role in protecting the PCB and facilitating efficient assembly. One of the essential finishing steps is the application of a solder mask. The solder mask is a protective layer that covers the copper traces, preventing oxidation, solder bridging, and environmental damage. It also provides insulation between adjacent traces and pads.
Surface finish technologies are used to enhance the solderability of the PCB and facilitate the soldering process during assembly. JLCPCB offers HASL (leaded/lead-free), ENIG, and OSP (with OSP mainly for copper-core boards; FR-4 boards support all three, while 6+ layers and RF boards typically use ENIG). HASL involves immersing the PCB in a bath of molten solder, followed by hot air leveling to remove excess solder, leaving a uniform coating on the copper surfaces. This method is cost-effective and widely used in the industry. ENIG is a popular surface finish for its excellent solderability and corrosion resistance. It involves depositing a thin layer of nickel followed by a layer of gold on the copper surfaces. The gold layer provides a reliable surface for soldering and ensures good electrical contacts. OSP is a surface finish that involves applying an organic compound to protect the copper surfaces during storage and assembly. It is cost-effective and environmentally friendly, but it may require additional steps to ensure good solderability.
HASL involves immersing the PCB in a bath of molten solder, followed by hot air leveling to remove excess solder, leaving a uniform coating on the copper surfaces. This method is cost-effective and widely used in the industry.
ENIG is a popular surface finish for its excellent solderability and corrosion resistance. It involves depositing a thin layer of nickel followed by a layer of gold on the copper surfaces. The gold layer provides a reliable surface for soldering and ensures good electrical contacts.
OSP is a surface finish that involves applying an organic compound to protect the copper surfaces during storage and assembly. It is cost-effective and environmentally friendly, but it may require additional steps to ensure good solderability.
Legend printing is another finishing step that involves adding identification markings and component references on the PCB. These markings facilitate assembly and troubleshooting processes. Legend printing can be achieved using methods such as screen printing or inkjet printing.
By selecting the appropriate finishing techniques, you can protect your PCB from environmental and mechanical stresses while enhancing its functionality and reliability during assembly and operation.
Advanced Manufacturing Techniques: Pushing the Boundaries
In addition to the fundamental steps of PCB manufacturing, there are advanced techniques that have revolutionized the industry and enabled the production of more complex and high-performance PCBs.
Multilayer PCB fabrication is a technique used when the circuit design requires more than two layers of copper traces. JLCPCB supports multilayer PCBs from 1 to 32 layers with controlled impedance available for 4+ layers (tolerance ±10%). Multilayer PCBs are created by laminating multiple layers of substrate material with copper foils in between. Each layer is patterned with the desired circuitry, and vias are drilled to establish electrical connections between the layers. The stack-up and arrangement of layers are carefully designed to ensure signal integrity, power distribution, and thermal management. Multilayer PCBs allow for increased circuit density, reduced size, and improved electrical performance, making them suitable for advanced applications such as high-speed communication systems, computer motherboards, and complex electronic devices.
Surface Mount Technology (SMT) is another significant advancement in PCB manufacturing. SMT involves mounting electronic components directly onto the surface of the PCB, as opposed to through-hole components that require leads passing through drilled holes. SMT components are typically smaller, lighter, and more efficient, allowing for higher circuit densities and improved signal integrity. SMT components are placed on the PCB using automated assembly machines, which increase the speed and accuracy of the assembly process. SMT has become the standard in most electronic devices due to its cost-effectiveness, reliability, and compatibility with modern manufacturing techniques.
These advanced manufacturing techniques require specialized equipment, skilled operators, and careful design considerations. By leveraging multilayer PCB fabrication and SMT, you can achieve compact, high-performance PCB designs that meet the demanding requirements of modern electronics.
Quality Control Measures and Inspection Methods
Quality control is a critical aspect of PCB manufacturing to ensure that the final product meets the highest standards of performance and reliability. Several quality control measures and inspection methods are employed throughout the manufacturing process to detect and prevent defects.
Visual inspection is the initial step in quality control, where trained personnel visually inspect the PCBs for any visible defects. This includes checking for proper alignment of components, solder joints, solder mask coverage, and any physical damage or anomalies.
Automated Optical Inspection (AOI) is a more advanced inspection method that utilizes high-resolution cameras and sophisticated software algorithms to inspect PCBs for defects. AOI systems capture images of the PCB and compare them with the expected design parameters. It can detect issues such as missing components, misaligned components, solder joint defects, and incorrect polarity. AOI provides faster and more accurate inspection results compared to manual visual inspection.
X-ray inspection is employed to examine hidden internal features of the PCB, such as vias, BGA (Ball Grid Array) solder joints, and inner layers. X-ray inspection allows for non-destructive testing and provides valuable information about the quality and integrity of the solder joints, especially in complex or high-density designs.
In-circuit testing (ICT) is performed on assembled PCBs to verify the electrical functionality of individual components and connections. ICT involves the use of specialized test probes that make contact with specific test points on the PCB. By applying controlled voltages and currents, the ICT system can identify faulty components, open or short circuits, and other electrical issues.
Functional testing is the final step in quality control, where the assembled PCB is tested under real-world operating conditions to ensure its functionality and performance. Functional testing may involve simulating different inputs and measuring the corresponding outputs to verify the proper operation of the PCB.
By implementing robust quality control measures and inspection methods, PCB manufacturers like JLCPCB can ensure the delivery of high-quality and reliable PCBs that meet customer expectations and industry standards.
Conclusion:
The process of PCB manufacturing involves several intricate steps, from substrate selection to layer imaging, etching, finishing, and quality control. Each stage plays a crucial role in creating high-quality PCBs that meet the requirements of modern electronics.
JLCPCB, with its advanced manufacturing capabilities and commitment to quality assurance, is a trusted partner in bringing your PCB designs to life.
Unlock the full potential of your electronic designs by partnering with us. With JLCPCB as your trusted manufacturing partner, you can confidently bring your innovative ideas to fruition and make a lasting impact in the world of electronics!
Q: What substrate materials does JLCPCB offer?
JLCPCB provides standard FR-4 (Tg 130°C/155°C), polyimide (PI) for flexible PCBs, and Rogers/PTFE materials for high-frequency applications.
Q: What is the maximum number of layers JLCPCB can manufacture?
JLCPCB supports up to 32-layer multilayer PCBs, with controlled impedance (±10%) available for 4+ layers.
Q: Which surface finishes are available?
JLCPCB offers HASL (leaded/lead-free), ENIG, and OSP. ENIG is recommended for 6+ layers and RF boards.
Q: How does JLCPCB ensure PCB quality?
Through visual inspection, AOI, X-ray, in-circuit testing (ICT), and functional testing at every stage.
Keep Learning
Understanding SMT PCB Boards Technology: An Essential Component of Modern Electronics
Surface Mount Technology (SMT) has changed manufacturing of modern electronics. It has made designs and assembly methods more efficient. Many modern electronics depend on SMT PCB boards, which make it possible for circuit designs to be small and efficient. This is what today's technology needs. This article discuss about many types of SMT PCB boards, their uses, and the best methods for designing and assembling them. 1. What is an SMT PCB Board? Printed circuit boards called SMT PCB boards, use surfac......
How to Choose the Right Prepreg Material for Reliable Multilayer PCB
Have you ever wondered what makes all those copper layers stick to a cross-section of a multilayer PCB? Prepreg material is the answer, and it is of much more importance than most engineers think it is. Choose the prepreg selection wrong, and you are predetermined to delamination, impedance drift, and long-term reliability problems. Prepreg is not only glue. It is a designed composite that determines your dielectric separation, dictates your impedance, affects signal loss, and determines your board be......
Via Filling Explained: Key Techniques, Benefits, and Solutions for High-Performance PCBs
Key Takeaways Via filling completely fills plated through-holes and microvias with epoxy or conductive copper paste, followed by planarization and copper capping (POFV). It eliminates voids, solder wicking, and thermal/mechanical issues while enabling reliable via-in-pad designs. Benefits include superior heat dissipation (up to 8 W/m·K), better signal integrity, higher mechanical strength, and improved assembly yields. JLCPCB provides free non-conductive filling + POFV on 6+ layer boards. Ideal for H......
How Fiducial Markers Guarantee Perfect Alignment in Professional PCB Fabrication
Today, the most sophisticated pick-and-place machine can place a 0.5 mm pitch QFP on its footprint, board after board, thousands of times, and never miss. It is not only a matter of expensive cameras or high-quality servos, but it begins with a little, very small copper dot, simply hanging there in the corner of your PCB. That dot represents a fiducial marker, and without it, even the smoothest SMT line would be laying components in the dark. The unrecognized heroes of automated assembly are the fiduc......
Technical Guidance: Character Design Specifications
To facilitate component assembly, future maintenance, and traceability of PCB manufacturing information (such as manufacturer, production date, batch number, etc.), various character markings are typically silk-screened onto the PCB. These include component designators, polarity marks, test point labels, company logos, and production traceability information. Traditional PCB character silk-screening uses the screen printing process, hence the term “silk-screen characters.” High-definition characters a......
Step-by-Step Guide to the Printed Circuit Board Manufacturing Process
Key Takeaways Core Role: PCBs provide the physical foundation and electrical connections for modern electronics. Multi-Step Process: Manufacturing spans design imaging, substrate creation, inner/outer layer etching, lamination, and surface finishing. Precision & Quality Control: Features micro-drilling (down to 100 µm) for layer connectivity, Automated Optical Inspection (AOI), and final electrical testing. Protection & Finish: Solder masks and surface finishes (e.g., ENIG, HASL) protect copper traces......