This website requires JavaScript.
Coupons
Ship to
Help Center
JLCPCB PCBA Review Before Payment Service Is Now Available

JLCPCB PCBA Review Before Payment Service Is Now Available

Last updated on Sep 23, 2026

Note

To improve the PCBA ordering experience, JLCPCB has officially launched the Review Before Payment service.

With Review Before Payment, your order can be reviewed before payment. Once the review is completed, the system will update the amount due based on the final review results. You can then confirm the final cost and complete the payment.

Review First, Pay Later for Clearer Costs

Submit Order → Complete Review → Confirm Final Cost → Complete Payment

After selecting Review Before Payment, you do not need to make an immediate payment when submitting your PCBA order. The order will first enter the review process.

During the review process, if there are cost changes resulting from component replacement, BOM/CPL file adjustments, or changes in Advanced Options fees, the system will update the final amount due before payment. You only need to pay the final amount after review — no additional payments or refunds needed afterward.

Key Benefits of Review Before Payment

1. More Flexible Payment

You do not need to pay immediately after submitting your order. Complete the review, confirm the final cost, and then make the payment.

2. Confirm Costs Before Payment and Avoid Additional Payments or Refunds

If the cost changes during the review, the system will directly update the amount due before payment. You can complete the payment once based on the final cost.

3. Components Are Reserved to Secure Your Order

Components are reserved as soon as the order is submitted and can be held for up to 7 days before payment, reducing the risk of inventory being released and the reserved components being purchased by other customers while your order is under review.

4. Easier Advanced Options Review

Advanced Options can be reviewed as soon as you submit your order. If the review results in any changes to the fees, the updated amount will be shown before payment, so no additional payment or refund is required afterwards.

How to Use

1. Select a Payment Method

Select Review Before Payment on the checkout page.

review before payment

2. Submit Your Order

After submission, the order enters the File Review status. You do not need to make an immediate payment.

file review

3. Wait for the Review

The review process proceeds through the following stages:

Pending Review → Reviewing → Review Completed

If the cost changes during the review, the system will update the amount due directly before payment.

review before payment submission

4. Pay After the Review Is Approved

After the review is completed and the order is Approved, the order moves to Awaiting Payment. Confirm the final cost and complete the payment.

pay after the review is approved

5. Enter the Regular Order Process

Once payment is completed, the order status changes to Confirmed. The order then proceeds through the regular PCBA process, with production files prepared before manufacturing begins.

pay your pcba order

Important Notes

  • Components are reserved immediately after a Review Before Payment order is submitted and can be held for up to 7 days before payment.
  • Orders that have been Approved but are still Awaiting Payment cannot be modified.
  • The review only covers costs confirmed before payment. If additional charges arise for other reasons after payment and the order has entered production, they will need to be handled separately and are not included in this review.
Try Review Before Payment for Your PCBA Order

Place your PCBA order now and select Review Before Payment on the checkout page for a more flexible and transparent review and payment experience.

Order Now