Mastering Thevenin’s Theorem: Practical Circuit Analysis
5 min
- What Thevenin's Theorem States:
- Steps to Analyze an Electric Circuit using Thevenin's Theorem
- Examples of Thevenin's Theorem:
- Conclusion:
We have seen the schematics of different circuits in the previous articles. When it comes to circuit solving then some predefined theorems are used. Just because at a higher level circuits become too complex, and we can not solve them just by looking at them. That's why to solve these complex systems, theorems are developed. One of the most popular ones is Thevenin’s Theorem. It allows us to replace any complex linear network with a single voltage source (called Thevenin voltage, Vth) in series with a single resistance (called Thevenin resistance, Rth). This equivalent circuit is advantageous when you need to study the behavior of a circuit under different load conditions. Today in this blog, we will see how to solve the network using Thevenin’s theorem.
What Thevenin's Theorem States:
Any linear two-terminal network of voltage sources, current sources, and resistors can be replaced by an equivalent circuit consisting of a single voltage source (Vth) in series with a resistance (Rth).
- Vth (Thevenin Voltage): The open-circuit voltage across the terminals A and B.
- Rth (Thevenin Resistance): The resistance seen at the terminals with all independent sources turned off (voltage sources shorted, current sources opened). If dependent sources are present, a test source method is required.
Steps to Analyze an Electric Circuit using Thevenin's Theorem
1. Open the load resistor(RL).
2. Calculate/measure the open circuit voltage. This is the Thevenin Voltage (Vth). It is computed at the end of load by removing it.
3. Open all current sources and short all voltage sources.
4. Calculate /measure the open-circuit resistance. This is the Thevenin Resistance (Rth).
5. Redraw the circuit using the measured open circuit voltage (Vth) in Step (2) as the voltage source and the measured open circuit resistance (Rth) from Step (4) as the series resistance. Connect the load resistor removed in Step 1. This forms the equivalent Thevenin circuit of the original linear network or complex circuit shown in the figure above.
6. Find the Total current or load current flowing through the load resistor by using Ohm’s Law:
Examples of Thevenin's Theorem:
Let’s understand these by three practical examples, in which we solve the circuits using Thevenin theorem.
Example 1: Calculate the current (IL) through the load resistance.
Step 1: Remove the Load ( 10 Ω) as shown below in the image and find Vth.
When the 10 Ω load is removed, we’re left with two branches only:
- Branch 1: 10 V source in series with 4 Ω.
- Branch 2: 12 V source in series with 6 Ω.
Now the circuit has two sources opposing each other and connected in series through their resistors.
That means the loop is:
10V − 12V + I(4) + I(6)=0
So, Vth = VAB
= 6I - 12
= 6(0.2) - 12
= 1.2 - 12
= -10.8V [B is negative Polarity and A is positive Polarity]
Step 2: To find Rth, open all current sources and short all voltage sources. From the above circuit, open all current sources and then short the voltage sources. The equivalent circuit is:
So, Rth=2.4 Ω
Step 3: Connect the load as removed in Step 1. This forms the equivalent Thevenin circuit of the original linear network or complex circuit, as shown below:
Step 4: Calculate Load Current(IL)
So, IL = 0.871 A.
Example 2: Calculate Load Current(IL) through the 0.1 Ω resistor.
Step 1: Remove the Load ( 0.1 Ω) as shown below in the image and find Vth.
VTh = VAB
= -5 × 0.5 + 2 × 0.4
= -1.7V [B -ve and A +ve]
Step 2: To find Rth, open all current sources in the above circuit. The equivalent circuit is:
Rth = RAB
= 0.5 + 0.4 = 0.9 Ω
Step 3: Connect the load as removed in Step 1. This forms the equivalent Thevenin circuit of the original linear network or complex circuit, as shown below:
Step 4: Calculate Load Current(IL)
So, IL= 1.7 A.
Example 3: Determine Thevenin's equivalent across the terminals A and B.
Step 1: For a clear understanding, let us redraw the given circuit as shown below:
Step 2: To find VTh: For each loop, there are two resistors in series. Each loop is a simple series divider.
Left loop has the 20 V source driving 8Ω and 12Ω in series:
With I1 flowing down through the 12Ω: VA = I1 × 12Ω= 1 × 12= 12 V. (So node A is +12 V relative to the bottom reference.)
Right loop has the 10V source driving 9Ω and 1Ω in series:
With I2 flowing down through the 1Ω: VB= I2 × 1Ω= 1 × 1= 1 V.
=12 V - 1 V = 11 V.
Step 3: To find Rth: Short all voltage sources in the above circuit.
Rth= RA + RB
= 4.8Ω + 0.9Ω =5.7 Ω
Step 4: Thevenin's equivalent circuit is shown below:
From these examples, it becomes clear that Thevenin’s theorem can be used in circuits that can not be solved with a simpler approach. Whether the network has only resistors and a voltage source, or a mix of sources, or even dependent sources, the same process applies to all.
Conclusion:
Using Thevenin's theorem simplifies additive circuits, voltage dividers, and combined sources. The process remains the same whether or not you have dependent elements. Once you become familiar with the steps, you should intuitively replace large parts of a network with refined "clean" Thevenin equivalents. Any additional analysis will be faster and more intuitive. For engineers or students, mastering Thevenin's theorem is about acquiring a practical skill for real-world engineers, not an academic exercise.
Popular Articles
• Choosing the Best PCB Color-Enhancing Aesthetics and Functionality
• PCB Silkscreen: All You Need to Know
• The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
• Understanding Electrical Schematics: A Comprehensive Guide
• PCB Board Design: A Step-by-Step Guide for Beginners
Keep Learning
A Beginner's Guide to Basic Electronic Components: Functions, Symbols & Uses
Every circuit, from a simple LED flashlight to a microcontroller board, is built from the same handful of common electronic components. This guide breaks down the ten basic electronic components you will encounter most often: What each component does How it works Key specifications Where engineers use it By the end, you will be able to recognize these electronic circuit components on a schematic, a PCB, or a parts bin, and know exactly why each one is there. These electronic components are the buildin......
Capacitor Voltage Rating Explained with Examples
Capacitors are small components widely used not only for power delivery but also for signal conditioning in electronic circuits. In this article, we focus on the capacitor voltage rating across different types of capacitors. At first glance, capacitors look simple—small cans, discs, or chips on a PCB. However, their markings carry essential design information, including capacitance and voltage rating. These are not arbitrary values but directly affect circuit reliability. Ignoring the voltage rating w......
From Prototype to Product with a Better Development Board
Note Prototype Fast: Development boards integrate power, clock, and programming circuits to validate firmware in hours. Pick the Right Platform: Use ESP32 for Wi-Fi/BLE, Arduino UNO for 5 V sensors, Raspberry Pi Pico for tight I/O timing, and Raspberry Pi 5 for Linux. Scale to Custom PCB: Reuse your prototype's certified module, firmware, and support circuits, but remove unused headers to cut unit cost. Build for Production: Use a 4-layer ground-plane stackup for wireless boards, verify BOM stock earl......
4 Layer vs 6 Layer vs 8 Layer PCB: How to Choose the Right Stackup
Random selection of layers in electronics may lead to serious signal integrity issues. That's why we always design our stackup before designing the PCB. Stackup decides the type of PCB and how it gonna perform under high-frequency conditions. There are a lot of things that directly affect the stackup of the PCB, related to impedance matching, routing density, signal and power integrity, electromagnetic compatibility (EMC), and cost. Knowing the requirements before design and the most critical componen......
Choosing the Best PCB Color-Enhancing Aesthetics and Functionality
Key Takeaways Choosing the best PCB solder mask color involves balancing aesthetics, visibility, and functionality. Green remains the top choice for superior contrast and inspection, while black offers premium appeal, white excels in LED applications, and other colors like purple and red provide unique design options. The ideal color depends on your priorities in inspection ease, thermal performance, and brand image, with minimal impact on electrical performance when using proper silkscreen contrast. ......
Single-Sided PCB Design: Combining Simplicity with Sophistication
Key Takeaways Single-sided PCBs offer a simple, cost-effective solution for many electronic applications. SMT and THT components require different mounting and soldering arrangements. Proper layer orientation, Gerber files, and design rules help ensure manufacturability. Aluminum PCBs require careful attention to insulation, component mounting, and silkscreen placement. A printed circuit board (PCB) provides mechanical support for electronic components and establishes the electrical connections requir......