The Importance of High Precision in PCB Stencil Manufacturing
3 min
- Understanding PCB Stencils
- The Need for High Precision
- Example: JLCPCB Stencil with Small Pitch Components
- Measuring Precision with a Digital Microscope Camera
- Conclusion JLCPCB
PCB stencils play a crucial role in the manufacturing process, especially when dealing with small pitch components. High precision in stencil manufacturing ensures accurate solder paste deposition, which is essential for reliable and high-performance electronic assemblies. In this article, we will highlight the importance of high precision in stencil manufacturing using an example from JLCPCB. We will also demonstrate the exact manufactured dimensions compared to the desired dimensions using measurements taken with a digital microscope camera.
Understanding PCB Stencils
PCB stencils are thin sheets made of metal (usually stainless steel) or polymer that have apertures cut into them. These apertures correspond to the pads on a PCB where solder paste needs to be applied. The stencil is placed over the PCB, and solder paste is applied through the apertures, leaving precise amounts of paste on the pads. This process is critical for the placement and soldering of surface-mount components.
The Need for High Precision
High precision in stencil manufacturing is vital for several reasons:
1. Accurate Solder Paste Deposition: Precise apertures ensure the correct amount of solder paste is deposited, which is crucial for forming reliable solder joints.
2. Minimized Solder Bridging: Accurate apertures reduce the risk of solder bridging between pads, which can cause short circuits.
3. Consistent Quality: High precision stencils contribute to consistent quality across multiple boards, reducing defects and rework.
Example: JLCPCB Stencil with Small Pitch Components
To illustrate the importance of high precision in stencil manufacturing, we ordered a PCB stencil from JLCPCB designed for a board with small pitch components. We will compare the desired dimensions of the stencil apertures with the actual manufactured dimensions using a digital microscope camera.
JLCPCB Stencil with Small Pitch Components
Measuring Precision with a Digital Microscope Camera
Using a digital microscope camera, we can capture high-resolution images of the stencil apertures and measure their dimensions. This allows us to verify the precision of the stencil manufacturing process.
Desired Dimensions vs. Actual Dimensions
For our example, we used a part MHPA0606RGBDT, which is a small LED with a pad size of 0.3mm x 0.3mm. Using a digital microscope camera, we will compare the desired dimensions of the stencil apertures with the actual manufactured dimensions.
Desired Dimensions:
· Pad Size: 0.3mm x 0.3mm
Desire Dimensions from part footprint
We will measure the actual dimensions of the stencil apertures for the MHPA0606RGBDT LED to ensure they match the desired specifications.
Results and Analysis
After capturing the images and measuring the apertures with the digital microscope camera, we found the following actual dimensions:
Actual Dimensions:
· Pad Size: 0.3098mm x 0.2980mm
These results show that the actual dimensions are very close to the desired dimensions, with only minor deviations. The deviations are within acceptable tolerances, demonstrating high precision in the stencil manufacturing process. This level of precision ensures accurate solder paste deposition, which is critical for the reliable performance of the assembled PCB.
Measured Dimensions of Stencil Apertures
Conclusion JLCPCB
High precision in PCB stencil manufacturing is essential for reliable and high-quality electronic assemblies. As demonstrated with the JLCPCB stencil example for the MHPA0606RGBDT LED, advanced manufacturing techniques and quality control measures can achieve the necessary precision even for small pitch components. By using tools like a digital microscope camera to verify dimensions, we can ensure that the stencils meet the required specifications and contribute to the overall success of the PCB assembly process.
Keep Learning
How to Choose an SMT Stencil
What is an SMT stencil? SMT Stencil is a thin metal sheet used in the soldering process for SMT (Surface Mount Technology) and it plays an essential role in the SMT soldering process. Smt Stencil allows the direct placement of solder paste onto the SMD pads of PCB, which can help prevent errors and defects during the reflow soldering process. This results in a precise amount of tin coverage once the work is completed. Types of SMT Stencils Depending on the application of solder paste, there are three ......
DIY PCB Stencil: How to Make a Solder Paste Stencil
Key Takeaways DIY is possible: You can make a working solder paste stencil from Kapton, Mylar, or vinyl using a craft knife, vinyl cutter, or laser for larger SMD components and low-volume prototyping. 0.5 mm pitch is the practical boundary: DIY stencils work well above 0.5 mm pitch but struggle with finer QFNs, QFPs, and BGAs due to poor aperture quality and paste release. Match thickness to your smallest pad: Use 0.10–0.15 mm (4–6 mil) sheet stock, choosing thinner material for smaller pads and thic......
Order Custom Stencils for PCB Assembly: How to Make, Buy, and Choose the Right Supplier
Surface Mount Technology (SMT) stencils are essential tools in modern PCB assembly. They are thin sheets of metal, usually stainless steel, with precise cut-outs that allow solder paste to be applied accurately to PCB pads. The quality of the stencil directly affects solder paste deposition, which in turn impacts the reliability of the final assembled PCB. Engineers often need to order custom stencils instead of relying on generic options. Every PCB design has unique pad layouts, component densities, ......
Custom Stencils for PCB Assembly: Design, Ordering, and Usage Guide
Have you ever faced solder bridging or insufficient solder issues that ruined an entire production batch? In many cases, the problem is not the pick-and-place machine, but the very first step of the process: solder paste printing. This is where custom stencils make the difference between a reliable product and one that requires extensive rework. Unlike rigid standard stencils, a custom SMT stencil gives engineers full control over solder paste volume, allowing precise adjustment to match increasingly ......
SMT Stencil Thickness Guide 2026: How to Choose the Right Solder Paste Stencil
In SMT assembly, the stencil quietly decides whether a production run succeeds or fails. Problems like bridging, tombstoning, and insufficient wetting are frequently traced back not to PCB design errors, but to incorrect stencil selection or poorly controlled paste volume. Quick Answer: How to Choose a Solder Paste Stencil If you need to define your stencil parameters immediately, follow this quick decision guide: Select thickness based on component pitch: Use component density as your primary baselin......
Custom Cut Stencils for PCB Assembly: How to Cut, Use and Choose the Right PCB Stencil
Custom-cut stencil and Solder paste printing are two of the most vital processes in Surface Mount Technology (SMT) PCB assembly, concerning solder joint quality, electrical performance, and product reliability over time. SMT stencils are used to deposit solder paste in accurate amounts onto PCB pads, or for depositing and compressing adhesive pastes which are arranged in the form of a column on components such as connectors and sockets. While PCB designs have seen a trend toward increased density, fin......