Blog - JLCPCB
PCB DesignPCB ManufacturingPCB KnowledgePCB Assembly
Blind vs Buried Vias: A Comprehensive Guide for PCB Design
A printed circuit board (PCB) is made up of layers of copper foil circuits stacked on top of each other, and the connections between different circuit layers rely on vias. If the holes drilled by a drilling machine or laser are left as is, they will not conduct electricity, because the surface of the original drilled hole is only resin, which is not conductive. Therefore, a layer of conductive material (usually copper) must be plated on the surface of the drilled hole. In this way, current propagates ......
Sept 20, 2024
Understanding Signal Reflection and Impedance Control in PCB Design: Key Techniques and Tools
Whenever a signal is sent digitally from one point to another, it changes the state of a signal line. The change in state of the signal can be described as an electromagnetic wave as it moves through the circuit. Reflection in the signal occurs when an electromagnetic wave encounters a boundary from one medium to the next. When the wave meets the boundary, part of the energy is transmitted as a signal and part of it is reflected. The process will continue indefinitely until the energy is absorbed by t......
Sept 21, 2024
PCB Impedance Control: Ensuring Signal Integrity in High-Frequency Circuits
Impedance measures the opposition of an electric circuit when alternating current is applied to it. It is the combination of the capacitance and the induction of an electric circuit at high frequency. Impedance is measured in Ohms, similar to resistance. If the impedances are different, reflections and attenuation occur that deteriorate the signal. For high-frequency analog or digital circuits, it is essential to protect the signals that propagate on the PCB from being damaged. In fact, signals above ......
Sept 21, 2024
Blind vs Buried Vias: A Comprehensive Guide for PCB Design
A printed circuit board (PCB) is made up of layers of copper foil circuits stacked on top of each other, and the connections between different circuit layers rely on vias. If the holes drilled by a drilling machine or laser are left as is, they will not conduct electricity, because the surface of the original drilled hole is only resin, which is not conductive. Therefore, a layer of conductive material (usually copper) must be plated on the surface of the drilled hole. In this way, current propagates ......
Sept 20, 2024
Flex PCB Design Tips and Tricks
Flexible printed circuit boards (Flex PCB) are a type of printed circuit board that is made from a flexible material, such as polyimide. FPCBs are used in a wide variety of applications, including consumer electronics, medical devices, and automotive electronics. flex PCB from jlcpcb Designing FPCBs can be challenging, as there are a number of unique considerations that must be taken into account. In this article, we will discuss some of the most important flex PCB design tips and tricks. The outline ......
Aug 27, 2024
FPC Panelization Design Standards and Requirements
FPC (Flexible Printed Circuit Board ) panelization is the process of arranging multiple FPC boards onto a single panel for efficient production. Proper panelization is crucial for optimizing material utilization, reducing production costs, and ensuring product quality. This article provides comprehensive FPC panelization design standards and requirements to guide engineers in creating optimal panel designs. General Panelization Guidelines Irregularly Shaped Frames: For irregularly shaped FPC frames, c......
Aug 27, 2024
Understanding Electrical Schematics: A Comprehensive Guide
Electrical schematics are essential for understanding and troubleshooting electrical systems. Whether you're an electrician or an engineering student, learning to read schematics is a valuable skill. What is an Electrical Schematic? An electrical schematic is a graphical representation of an electrical circuit, using standardized symbols to depict components and their connections. Schematics convey the circuit's design and function, making it easier to understand how it operates Symbols are the founda......
Aug 23, 2024
Common problems and solutions in PCB design
PCB (Printed Circuit Board) design is a crucial aspect of electronic product development. During the design process, we often encounter challenging issues, which may include circuit design and wiring regulations. Understanding these common problems and their solutions can help engineers enhance the quality and efficiency of the design. Unreasonable circuit layout Circuit layout is crucial for maintaining signal integrity and electromagnetic compatibility. Unreasonable layout can lead to issues such as......
Aug 9, 2024
Navigating the Impedance Landscape: Selecting the Right Impedance for USB, Ethernet, HDMI, and SD Card Interfaces
1- Introduction: In the realm of high-speed digital communication, choosing the right impedance is a critical aspect of successful PCB design. Impedance matching ensures optimal signal integrity, minimizes reflections, and enhances the overall performance of interfaces such as USB, Ethernet, HDMI, and SD Card. In this blog post, we'll explore the importance of impedance, the factors influencing impedance selection, and best practices for ensuring reliable data transmission in these widely used interfa......
July 17, 2024
The Importance of Using Optocouplers in PCB Design
In PCB design, ensuring the protection and reliability of microcontroller signals is paramount. One of the most effective ways to achieve this is by using optocouplers. These components provide optical ground isolation, which is crucial for protecting sensitive microcontroller signals from high-voltage circuits and noise. This article explores the importance of using optocouplers in PCB design and highlights the variety of optocoupler models available in the JLCPCB parts library. What is an Optocouple......
July 13, 2024
The Importance of Using ISP Programming Ports in PCB Design
In the world of PCB design, optimizing space and reducing costs are always top priorities. One effective way to achieve these goals is by incorporating In-System Programming (ISP) ports directly onto the PCB. ISP ports allow for programming the microcontroller or other programmable devices on the board without the need for permanent programming port components. This article highlights the importance of using ISP programming ports in PCB design and discusses how they help save costs and reduce board si......
July 13, 2024
Light-Emitting Diodes (LEDs)
Light-Emitting Diodes (LEDs) have become a cornerstone in modern electronics, illuminating everything from household lighting to complex industrial systems. Their integration into Printed Circuit Boards (PCBs) is essential for various applications, providing efficient lighting solutions that are both versatile and reliable. This article explores the fundamental aspects of LEDs, their history, types, applications, and the critical considerations when designing PCBs that incorporate LEDs. What is an LED......
June 25, 2024
Understanding the Importance of Annular Rings in PCB Design
Annular rings play a crucial role in printed circuit board (PCB) design, ensuring the proper electrical connection of two pads. The signal and current flow are characterized based on the placement of annular rings between two layers. Incorrect calculation of size and improper placement can lead to transient behavior and flicker noise in electronic components. In this article, we will consider all important steps to improve our design from annular ring issues, tangency, and breakout. An annular ring in......
June 13, 2024
45 Must-Know Flex PCB Design Tips You Can't Afford to Miss!
Achieving perfection in product design requires a careful balance between meeting design requirements and manufacturing standards. However, when it comes to flex PCB (FPC) design, many engineers find themselves at a loss, unsure of where to begin. In this insightful guide, we will delve into 45 essential design guidelines for FPC. By the end, you'll have the knowledge and confidence to navigate the complexities of flex PCB design. Outline and Drilling 1. The minimum distance from through-holes to the ......
June 12, 2024
Precision in Propagation: Navigating Length Matching and Tuning for Single Tracks and Differential Pairs
In the intricate world of high-speed PCB design, achieving precise signal integrity is paramount for seamless data transmission. Length matching and tuning play pivotal roles in ensuring that signals, both single-ended tracks and differential pairs, reach their destinations without distortion or timing issues. In this blog post, we will delve into the importance of length matching, the challenges associated with it, and best practices for tuning both single tracks and differential pairs in your PCB la......
May 29, 2024
Shielding in PCB Design: Ensuring Signal Integrity and Electromagnetic Compatibility
Printed Circuit Board (PCB) design plays a pivotal role in determining the performance and reliability of electronic devices. As technology advances, the demand for high-speed data transmission and increased electronic complexity grows. To meet these challenges, engineers are turning to effective shielding techniques in PCB design. In this blog post, we'll delve into the importance of shielding, its benefits, types of shielding, and best practices for implementation. The Significance of Shielding In t......
May 27, 2024
Enhancing PCB Reliability: A Deep Dive into VIA-in-PAD Design
Printed Circuit Board (PCB) design is a critical aspect of electronic product development, and engineers continually seek innovative solutions to improve performance, reliability, and miniaturization. One such design technique gaining prominence is VIA-in-PAD (VIP) implementation. In this blog post, we'll explore the significance, advantages, challenges, and best practices associated with VIA-in-PAD in PCB design. What is VIA-in-PAD? VIA-in-PAD refers to the practice of placing vias directly within th......
May 23, 2024
Achieving Harmony in Mixed-Signal PCB Design
In the electronic world, it's now common to mix analog and digital parts on one board due to changes. Mixed-signal PCB design represents a harmonious marriage of analog and digital worlds, unlocking a myriad of possibilities for sophisticated electronic devices. This blog post will talk about mixed-signal PCB design. It will cover the challenges, best practices, and important factors for achieving optimal performance. The Essence of Mixed-Signal Design Mixed-signal design refers to the integration of ......
May 20, 2024
Innovating PCB Design: Leveraging DFM Principles for Enhanced Functionality and Manufacturing Efficiency
In the realm of electronics manufacturing, the initial design phase stands as a pivotal determinant of project success. For PCB (Printed Circuit Board) designers, integrating Design for Manufacturing (DFM) principles into their workflow is paramount. These principles ensure efficient, cost-effective manufacturing with uncompromising quality. Essential guidelines, from component selection to testing, guide designers to optimize their designs for manufacturing efficiency and excellence. I. Component Sel......
May 17, 2024
Designing Effective PCB Antennas for Wireless Communication Systems
In the world surrounded with the wireless communication, the demand for compact, inexpensive and reliable antennas has never been higher. One of the solutions for this problem can be usage of Printed Circuit Board (PCB) antennas. Using PCB antennas represents a convenient solution for integrating them directly into electronic devices, eliminating the need for bulky external antennas. In this article, let’s explore the approach to PCB antenna design, key considerations and best practices for achieving ......
May 10, 2024
Understanding Analog and Digital Ground in PCB Design
When working on printed circuit board (PCB) design, proper grounding is crucial for ensuring signal integrity, minimizing noise, and maintaining reliable performance. Two common types of ground planes used in PCB layouts are Analog and Digital ground. In this article, we will explore the differences between analog and digital ground, their significance in PCB design, and best practices for their implementation. 1. Analog Ground vs. Digital Ground Analog ground and digital ground have separate purposes......
May 10, 2024
- 1
- 2
- 3
- 4