Simplified yet Intricate: Single-Sided PCB Design
3 min
- Structure of Single-Sided PCB
- Soldering of Single-Sided PCBs
- Designing Engineering Files
- Characteristics of Factory Production
- Special Note
- Conclusion
Printed Circuit Boards (PCBs) are crucial electronic components. They act as the support structure for electronic devices and serve as the carrier for electrical connections among electronic components. Since its inception in 1925, the evolution of printed circuit boards has led to increasingly intricate layouts, more layers, and greater complexity. However, even amidst these advancements, the most basic form known as the single-sided PCB is still widely employed in various industrial products like radios, washing machines, and remote controls.
Structure of Single-Sided PCB
Traditional FR4 single-sided PCBs accommodate one side of copper, one side of solder mask, and two sides of silkscreen (depending on customer design). Due to the absence of the electroplating step in the production of single-sided boards, the hole walls of these PCBs lack copper (note: board thicknesses of 0.4 mm, 0.6 mm, 0.8 mm, and 2.0 mm are produced by default as double-sided to maximize utilization of board material. For boards of these thicknesses, through-holes will be plated).
Soldering of Single-Sided PCBs
Given the structure of single-sided PCBs, where only one side contains circuitry, soldering is limited to the exposed pads on that particular side. Depending on the component's structure, this results in two distinct soldering methods:
1. Same-Side Soldering
For components where the main body is on the same side as the circuit, often used for SMT-type component soldering.
2. Opposite-Side Soldering
For components where the main body is on a different side from the circuit, commonly used for through-hole component soldering.
Designing Engineering Files
In practical design, a complete PCB is designed layer by layer.
Taking double-sided boards as an example, patterns designed on the top layer are seen directly (e.g., top layer text appears correctly). Conversely, patterns designed on the bottom layer have a mirroring effect; if text is designed on the bottom layer and it appears upright in the design software, due to the mirroring effect, the text on the actual board will appear reversed (since the physical board is viewed from the opposite side).
The same principle applies to the circuit layer. For single-sided boards, when designing circuitry on the bottom layer, because of the mirroring effect, the actual board needs to be viewed from the front with a backlight to match the bottom layer's circuit design (as shown in the figure below).
Characteristics of Factory Production
In actual production, to avoid burrs and peaks, the mirrored image of the bottom layer's wiring is used for the top layer (mirrored production does not affect the customer's original design structure). This approach ensures that the drill bit first penetrates the copper layer on top. Since the substrate provides support underneath, the copper can be drilled very cleanly. Drilling holes with the copper side facing down would result in numerous burrs and peaks.
Special Note
1. Single-sided aluminum-based boards have a conductive aluminum base layer, making them unsuitable for component soldering (soldering could lead to short circuits).
2. Single-sided aluminum-based boards generally have silkscreen printed on one side, applied to the copper-covered side. Printing Silkscreen on the aluminum-based side is not recommended as it may be difficult to read.
Conclusion
In summary, single-sided PCBs have a straightforward design, but careful attention must be paid to the layer where the circuit is located and where soldering occurs to avoid an unintentionally mirrored design.
Keep Learning
Why Via Aspect Ratio Is Critical for Reliable PCB Manufacturing
Have you ever received a PCB lot back with intermittent open circuits that do not present themselves until after reflow or thermal cycling? The underlying cause, in most instances, is the one parameter that was not given much attention: the aspect ratio of the via. It is among those figures that silently dictate the life or death of your plated through-holes in the real world, or that they will grow into time bombs lurking within your board. The via aspect ratio is a ratio between two basic physical d......
How Photodiode Differs from Phototransistor
For two centuries, light-sensitive devices have been widely employed, primarily for wireless applications. From the automatic street lamps to your television remote. Photodiodes and phototransistors are two of the most popular elements to make this happen. The main principle here is to convert light energy into electrical signals, and then these electrical signals are processed to take further action. However, the operational processes, signal types, and applications of photodiodes and transistors are......
What is Solder Mask and How Does it Impact Your PCB Designs?
Solder mask may not be the most exciting topic in PCB manufacturing, but it's definitely one of the most crucial. Without proper solder mask, your Printed Circuit Boards (PCB's) could suffer from shorts, bridges, corrosion, and other costly and time-consuming issues. So, if you want to ensure the quality, reliability, and longevity of your electronic products, you need to know everything about solder mask - from it's purpose and types to it's application and design implementations. In this ultimate gu......
Understanding Schematics: A Design Walkthrough
Every electronic design is based on a schematic diagram. The schematic diagram is the blueprint that shows how electronic components are connected to create a circuit. The schematics serve as a route map showing how current and signals will flow from the input stage to the output stage. Before a PCB (Printed Circuit Board) is actually made, we typically design a schematic. When it comes to the revision of the circuit, the main work is done first at the schematic level, and after that PCB is again modi......
PCB Basics 2: Design Guidelines
Welcome to the second article in our PCB Basics series. In this article, we will explore the essential PCB design guidelines that are crucial for achieving optimal PCB design performance and functionality. Whether you're an electronics enthusiast, hobbyist, engineer, student, or professional in the field, understanding these guidelines will empower you to create high-quality PCB designs. Let's dive into the details with JLCPCB! Component Placement: Effective component placement is vital for optimal PC......
Exploring IoT Applications with Raspberry Pi and PCB Design
The Web of Things (IoT) is impacting the manner in which we communicate with innovation. It alludes to the organization of actual gadgets, vehicles, home machines, and different things installed with hardware, programming, sensors, and availability, which empowers these items to interface and trade information. Because of its flexibility and minimal expense, Raspberry Pi, a little and reasonable PC, has turned into a well-known decision for IoT applications. In this article, we will investigate how Ra......