What is a Blank Circuit Board (Bare PCB) and How is it Used
7 min
- 1. Difference Between Zero PCB and Blank PCB:
- 2. Structure of a Bare PCB
- 3. How to Make a Blank PCB at JLCPCB
- 4. Types of blank PCBs:
- 5. Design Guidelines of a Mixed Signal Bare PCB:
- 6. Benefits of Using Blank PCB:
- Conclusion
A printed circuit board (PCB) that doesn't have any electronic parts on it is called a blank PCB, bare PCB. A PCBA, on the other hand, is a PCB that has all the electronic parts that it needs. Because there is a layer of copper covering the circuit board, blank PCB boards are sometimes called "copper clad" circuit boards. A blank PCB is a computer board that is made up of layers of epoxy fibreglass, copper foil, and PCB inks. Before the copper sheets, there are non-conductive prepreg layers on a blank printed circuit board. The board also has a base sheet. Copper-filled holes link the several layers of copper traces.
Single-sided, double-sided, and multi-layered bare PCBs are some of the different types. It is possible to choose the stackup based on its complexity and usefulness. To make them, they use base materials like FR-4 (fibreglass epoxy), polyimide (for flexible boards), or metal-core materials for heavy-duty uses. Some of the things will be talked about in the next section of this post. This piece talks about what a blank PCB is, what it can be used for, and how it is made. It also shows how to use JLCPCB's fabrication services to make a blank PCB.
1. Difference Between Zero PCB and Blank PCB:
A zero PCB (also called a general-purpose or perf board) is a pre-made board with a grid of holes and copper pads. It is used for manual circuit prototyping. Components are inserted into the holes and connected using wires or solder bridges. Zero PCBs are ideal for quick, small-scale experiments but do not support complex or high-density circuits.
A blank PCB, on the other hand, is a custom-manufactured board. It does not have pre-drilled holes or copper traces. It is fabricated according to a specific circuit design, for any shape, size, or number of layers. Blank PCBs are used for professional prototyping and production.
2. Structure of a Bare PCB
A typical blank circuit board consists of the following layers:
⦁ Substrate (Base Material): Provides mechanical support and insulation.
⦁ Copper Layer(s): Conductive pathways that interconnect electronic components.
⦁ Solder Mask: Protects copper traces and prevents solder bridging during component placement.
⦁ Silkscreen: Printed text or symbols indicating component placement and reference designators.
3. How to Make a Blank PCB at JLCPCB
JLCPCB is a widely used PCB fabrication service known for its affordability, fast turnaround, and comprehensive design-to-production workflow. Creating a blank PCB through JLCPCB involves the following steps:
1. Prepare Your Gerber Files
Design your circuit in a PCB design software such as KiCad, Altium Designer, or Eagle. Export the Gerber files, which include layer data for copper, solder mask, silkscreen, and drill information.
2. Visit the JLCPCB Website
Log in to your account and begin a new PCB order. Upload the Gerber files to their platform. The interface will automatically render a preview of your blank board layout.
3. Configure PCB Specifications
Choose your board properties, such as:
⦁ Dimensions and quantity
⦁ Number of layers
⦁ Board thickness
⦁ Copper weight
⦁ Surface finish (HASL, ENIG, etc.)
⦁ Solder mask color
Since you are ordering a blank PCB, you do not need to include a Bill of Materials (BOM) or pick-and-place files for component mounting.
4. Place the Order
Once all parameters are confirmed, proceed to checkout. Choose a shipping method based on your delivery timeline and budget.
5. Receive and Use Your Blank PCB
Upon delivery, your blank PCBs will be ready for component assembly—either manually or via an automated pick-and-place system, depending on your setup.
4. Types of blank PCBs:
1. FR-4
The most often used blank PCB is FR4 PCB. Although FR4 is level 4 flame retardancy rather than a substance.FR4 PCB is actually a fourth class flame retardant rated epoxy glass fibre PCB. Though it is partially cured, the pre-impregnated layer between the copper layers is likewise epoxy glass fibre.
Manufactured easily, FR4 blank PCBs are less expensive than other PCBs with the same number of layers and circuit complexity.
2. Metal core PCB
Copper and aluminium core PCBs are among metal core PCBs. Mostly utilised for LED lighting and other power applications, metal core PCBs offer far higher heat conductivity than FR4 cores.
3. Rigid-Flex PCB
PI or PET-based empty PCBs that can bend are flexible or rigid-flex PCBs. Special flexible PCBs, rigid-flex PCBs have laminated FR4 PCB layers on their flex region.
4. High Frequency PCB
Furthermore a high-speed and RF microwave PCB is a high-frequency PCB. Transmitting and receiving high-frequency signals, this PTFE-based blank PCB From radars to anti-collision systems to GPS to cellphones to missile systems, high-frequency PCBs find use in antennas, radars, etc.
5. Design Guidelines of a Mixed Signal Bare PCB:
Make Sections: When designing PCB wiring, the following principles should be followed: separating analog signals from clock signals, maintaining a separation of 20H between both sections. Where H refers to the spacing of the top layer to the next ground returning layer.
Impedance Matching: When completing PCB design, it is necessary to ensure that the PCB has uniform impedance and low electromagnetic interference. This will lower down the signal reflections and keep the proper signal integrity.
6. Benefits of Using Blank PCB:
First of all, it lets designers test circuits and try out new ideas at very little cost; once the circuit is perfect, it is then moved to a completed board for soldering and assembly. Second, DIY electronics aficionados extensively use bare PCBs since they can be made from scratch when a public PCB cannot fit your design requirements. Here are some primary advantages:
Modern electronics production depends on the diversity and adaptability of the blank PCB board, which is the pillar of circuit design and offers a strong basis for innovative electronic products.
Blank PCB Testing:
Shape and Size: Although rare, the bare PCB may already have flaws before components are introduced; failure of the PCB as a circuit board frame after installation can cause various issues.
Manufacturing Issues: Among the more often occurring issues are under-etching, over-etching, and holes. Manufacturing failures can result from even little flaws. Bare board testing becomes even more crucial as demand for multilayer PCB boards rises from growing component density.
The components of the board are the organs and muscles if the bare PCB is its skeleton. Since components can be somewhat costly and often vital, a strong frame helps to avoid long-term waste of high-end items.
Conclusion
Blank printed circuit boards are the basics of all electronics and electrical devices and products. Using services like JLCPCB, creating custom blank PCBs is more accessible than ever. With just a design file and a few configuration steps, users can transform a digital circuit layout into a tangible, production-ready board. Whether you're a professional engineer or an electronics enthusiast, understanding and utilizing blank PCBs is foundational to successful hardware development. If you have any questions about blank or bare printed circuit boards, such as stackup, layers or regarding any design issue, please contact JLCPCB support team.
Popular Articles
• Understanding the Basics of Electronic Devices and Circuits
• Understanding Digital Circuit Timing: Setup Time, Hold Time, Contamination Delay & Clock Skew
• PCBs Explained: A Simple Guide to Printed Circuit Boards
• Guide to the Top 10 Commonly Used Electronic Components
• Digital 101: Fundamental Building Blocks of Digital Logic Design
Keep Learning
Basic Bridge Circuits
Key Takeaways Core Principle: Bridge circuits (Wheatstone, Kelvin, H-Bridge, etc.) enable high-precision measurements and power control. Applications: Essential for sensor signal conditioning, AC/DC rectifiers, and motor drivers. JLCPCB Optimization: Maximize circuit stability with JLCPCB’s 3/3 mil traces, 4-layer stackups, and High-TG FR-4. A bridge circuit splits an input voltage into two paths, compares the voltages across different branches, and provides an output. These circuits are widely valued......
Understanding Industrial PCB Production:Materials, Manufacturing Processes, and JLCPCB Capabilities
Key Takeaways Layer Capabilities: Supports up to 32-layer Rigid and 28-layer HDI PCBs (Rigid-Flex unsupported). Industrial Materials: High-Tg FR-4 (Tg 170°C), Aluminum cores, and Rogers RF laminates. Free POFV Technology: Free resin-filled via-in-pad provided for 6–32 layer designs. Turnkey Assembly: Integrated online DFM checks and automated SMT assembly. Nearly all electronic devices rely on Printed Circuit Boards (PCBs) as their foundational backbone, supporting and interconnecting active and passi......
Selecting the Right PCB Board Prototype Approach for Rapid Product Testing
Key Takeaways Authentic Testing: Prototypes use production-grade materials, stackups, and footprints for realistic design validation. Ditch DIY: Breadboards and chemical etching fail on SMD parts, fine traces, and high-speed impedance. Early Defect Catch: DFM checks and flying probe tests eliminate short circuits, acid traps, and layout errors before build. High-Speed & Thermal: Critical signals need controlled impedance; heat-generating parts require thermal via arrays. Fast Delivery: Professional 24......
FR4 vs Rogers: Which PCB Material Should You Choose?
Traditionally, manufacturers have been making PCBs or printed circuit boards of materials that offer resistance to heat and are, therefore, less expensive to produce. As the electronics industry is increasing in terms of high frequency application, only FR4 is not enough. Some equipment, while not being subject to extreme temperatures, may have to work at RF or radio frequencies. According to the extreme performance conditions demanded by RF, specialized materials such as Rogers are necessary to deliv......
Optimize PCB Trace Spacing for High-Performance PCBs
Key Takeaways Trace Spacing vs. Clearance: Trace spacing is the edge-to-edge distance between copper conductors on the same layer, while clearance encompasses the broader safety envelope between traces and non-trace features like board edges and mounting holes. The 3W Rule: For high-speed signals, maintain at least 3x the trace width between centerlines (2W edge-to-edge spacing) to reduce crosstalk by up to 70%. IPC-2221 Standards: Industry-standard clearance values depend on voltage levels, altitude,......
A Deep Dive into Polyimide PCB Materials for High-Thermal Stability
Key Takeaways Two Form Factors: Available as flexible film (bends without cracking) or rigid glass laminate (structural stability). Extreme Heat Resistance: Handles operating temperatures over 200°C with a Tg up to 250°C-410°C. High Via Reliability: Expands only 1.2% in the z-axis (50°C to 260°C), preventing plated hole cracks. Mandatory Baking: Absorbs up to 2.8% water weight, requiring a pre-reflow bake to avoid delamination. JLCPCB Flex Support: Best for high-reliability uses; JLCPCB supports 1 to ......