Flexible PCB Material Selection Guide : Polyimide, PET, and Reliability Considerations
12 min
- Understanding Flexible PCB Materials
- Polyimide (PI) as the Standard Material for Flexible PCBs
- Polyimide vs PET in Flexible PCB Applications
- Reliability Considerations in Flexible PCB Material Selection
- Material and Manufacturing Considerations for Reliable Flexible PCBs
- JLCPCB's Flexible PCB Material and Manufacturing Capabilities
- Frequently Asked Questions (FAQ)
Key Takeaways
Choosing the right flexible PCB material directly impacts bending performance, thermal reliability, and product lifespan. This guide explains the differences between polyimide (PI) and PET materials, their applications, and key factors to consider when selecting flex PCB materials. With proper material selection and manufacturing control, engineers can achieve reliable flexible circuits for consumer electronics, industrial devices, and high-performance applications with JLCPCB.
Ever been curious about the ribbon cable behind a laptop hinge, peeked inside a fitness tracker, or folded open a smartphone? All of those products use flexible circuits, and the quality you hold in your hand begins with the proper Flexible PCB Materials. The substrate isn't just a passive carrier — it determines the number of bend cycles your board will endure, how it will tolerate heat, and whether it will crack in six months in a pocket. While a flex PCB may be perfectly fine on the bench, it can fail in the field just because the wrong flex PCB base film was selected.
The choice of material is a combination of mechanical engineering, thermal management, and cost control. Do it correctly, and your product will flex for years. In this guide, we will go over the most used flexible circuit materials, make a comparison between polyimide and PET head-to-head, and explore the reliability factors. By the end, you will be certain how to choose flexible PCB material without any hesitation.
Understanding Flexible PCB Materials
A Flexible printed circuit is constructed from a series of thin films and adhesives instead of the rigid glass-reinforced laminate used in standard boards. A base dielectric film supports the copper, an adhesive bonds the layers, and a protective coverlay seals it all. All are actual choices that have consequences. Whereas FR4 is a rigid substrate, flex circuits are a true menu of substrates. That freedom is great, but it can also lead to a bad decision that can be hidden in an otherwise good design.
Common Material Types Used in Flexible Circuits
Flexible circuits rely on a small but unique family of materials, all optimized for their respective requirements. To make a sound choice in flexible PCB materials, it is essential to grasp the contributions of each.
- Polyimide (PI): Industry workhorse, good thermal stability, good mechanical stability, and the default for soldered, high-reliability flex.
- Polyester (PET): A lower-cost film that is good for flexibility, but is not suitable for high temperatures; it is used in membrane switches and disposable electronics.
- Adhesives: Acrylic and epoxy-based bonding layers, which are used to join the stackup together; adhesiveless laminates are available for finer features.
- Copper foil: Rolled-annealed (RA) copper for dynamic bending applications, or electrodeposited (ED) copper for static applications.
- Coverlay and cover coat: Protective overcoat is usually of polyimide film with adhesive or a printed liquid photoimageable layer.
Why Material Selection Impacts Reliability and Flexibility
The entire idea of a flex circuit is that it flexes, and flexing causes cyclic stresses to be applied directly to the copper and the dielectric. A material that is not fatigue resistant has microcracks well before the board ages out. The dimensional stability (the amount of film shrinkage or movement during lamination/reflow) is also dependent upon the material. Too much movement makes openings and registration problems, as layers and pads become misaligned. Thermal tolerance is the third pillar. A film with a softening point of 150°C just won't hold up in an assembly that is lead-free reflowed at 245-260°C. The substrate thus stealthily defines the upper limit of all the processes and field conditions downstream.
Polyimide (PI) as the Standard Material for Flexible PCBs
Engineers refer to "flex PCB," and typically, they are talking about a circuit made on a polyimide substrate. Decades of use have proven the reliability of PI, making it the chosen base film. The answer is simple: polyimide is one of the few materials that offers a rare combination of high thermal stability, mechanical toughness, and chemical resistance – and in a film that is only 12.5 to 50 microns thick. There aren't many that match up to that whole spectrum.
Thermal Stability and Mechanical Performance of PI
The special feature of polyimide is its thermal resistance. It retains mechanical and dielectric properties at temperatures that are higher than the glass transition temperature of most other plastics. Polyimide flex film has the following important performance features:
- High thermal rating: For continuous use at 150°C and for a short time to temperatures up to lead-free reflow.
- Excellent flex life: when used in combination with rolled-annealed copper, it is able to resist hundreds of thousands to millions of bend cycles.
- High resistance to mechanical forces (tensile strength): will not tear or elongate when subjected to force.
- Good chemical resistance: withstands etchants, fluxes, and cleaning agents employed in fabrication.
- Stable Dielectric Constant: The dielectric constant of the material is typically in the range of 3.2 to 3.5, which provides stable impedance.
Why PI Is Preferred for High-Temperature Applications
Most flex circuits only endure the harshest thermal event: soldering. The reflow temperature of lead-free SAC305 is 245-260°C, which would instantly melt or warp a low-temperature film. Polyimide takes the rough and tumble in stride. It has a high decomposition temperature, maintaining its dimension and structure during reflow, wave soldering, and rework cycles. That is the only practical alternative to flex boards with soldered components. In addition to assembly, boards can be subjected to continuous heat from applications such as automotive under-hood electronics, LED lighting, and industrial sensors. The stability of polyimide under long-term thermal stress ensures reliable circuits throughout their lifespan.
Polyimide vs PET in Flexible PCB Applications
The most popular substitute for polyimide is PET (polyester), and whether to use one or the other is one of the most common decisions in the flexible PCB material selection process. They're both flexible, they're both readily available, but they're both used for very different purposes.
Temperature Resistance and Mechanical Durability Comparison
The most significant change is tolerance to heat. PET will soften and deform between 130-150°; it cannot be soldered in the traditional way. Conductive adhesives or crimped contacts are normally used in PET circuits. Polyimide also outperforms in mechanically related fatigue life and tensile strength, which makes it a safer choice for dynamic bending. Let's do a side-by-side comparison of the two films.
| Property | Polyimide (PI) | Polyester (PET) |
|---|---|---|
| Continuous use temperature | ~150°C | ~105-130°C |
| Solderability | Yes (reflow/wave) | No (conductive adhesive) |
| Flex/bend fatigue life | Excellent | Moderate |
| Tensile strength | High | Moderate |
| Dimensional stability | Very good | Moderate |
| Moisture resistance | Good | Good |
| Relative cost | Higher | Lower |
Cost and Application Trade-Offs
PET is also much less expensive than polyimide, and for the appropriate product, it is worth the price. It's simply a balance of selecting the proper material for the application.
- Use PET for membrane switches, keypads, single-use medical sensors, LED light strips, and more low-temperature, cost-sensitive products.
- Use polyimide for soldered assemblies, dynamic-flex, automotive, and aerospace electronics, and for applications where prolonged exposure to heat is involved.
It's not just about the price. For boards that require soldering and/or multiple bending, there is no choice but polyimide, no matter the price.
Reliability Considerations in Flexible PCB Material Selection
The selection of the base film is just the first step. Over the long term, the reliability of the material hinges on its ability to resist moisture, maintain its size during processing, and withstand mechanical stresses after applying a coverlay. These are the factors that distinguish a flex circuit that will last the life of the product from one that will fail after a few thermal cycles. Let's check out the ones that bite the most.
Moisture Resistance and Dimensional Stability
Polyimide is hygroscopic and will absorb moisture from the air, and that moisture will flash to vapor during reflow, which will result in delamination or popcorning. That is why flex boards always require baking prior to assembly. Dimensional stability is also of utmost importance. During etching, lamination, and reflow, the film expands and contracts, causing too much movement that results in loss of layer-to-layer registration. In the case of multi-layer flex, even slight dimensional drift between layers misaligns vias and pads. Choosing a film that has low and predictable shrinkage and controlling humidity during the process will result in high registration.
Coverlay Protection and Crack Resistance
A coverlay is the flexible version of a solder mask, which is a protective film typically made of polyimide with adhesive, and applied over the traces. It does more than just insulate; it also conveys the copper through the neutral bending axis to help minimize strain. Crack resistance is directly improved with a good coverlay design. With copper in the middle of the bend, maximum stress levels on the conductors are significantly reduced.
- Strain relief: Copper is placed close to the neutral axis with Coverlay placement to reduce bend stress.
- Environmental sealing: Keeps traces safe from moisture, chemicals, and abrasion.
- Crack mitigation: Improves flex area, tear resistance at bend points.
- Pad definition: Pads are only exposed where they need to be soldered, protecting the rest.
Material and Manufacturing Considerations for Reliable Flexible PCBs
The best of materials is worse if the manufacturing process cannot cope with it consistently. Matching material choices to a stable, well-controlled production flow is the cornerstone of reliable flex circuits. That's where design-for-manufacturing thinking becomes useful: The idea is to choose materials that your fabricator can work with without any unexpected surprises in the manufacturing process.
Stackup Compatibility and Process Stability
All layers within a flex stackup must be compatible. Different CTEs of the base film, adhesive, and copper can cause internal stress to manifest itself as warping or delamination after thermal cycling. These properties are kept in harmony in a stable stackup. When designing a flex stackup, take the following into account:
- Make sure to build it symmetrically: symmetric stackups resist curl and twist.
- Consider adhesive flow: adhesive squeeze-out during lamination should not exceed tolerance.
- Plan for transition zones: strengthen the rigid-to-flex border in rigid-flex designs.
DFM Checks and Material Quality Control
Design for Manufacturing (DFM) verifies that reliability issues are addressed prior to going into production. These reviews are specifically geared to bend radius, trace routing through flex zones, and coverlay registration for flex. The quality control of incoming materials is equally important. The film thickness, copper weight, and adhesive consistency are verified to ensure that each batch reacts in the same manner on the line.
Industry standards like IPC-6013 (qualification and performance specification for flexible printed board) and IPC-2223 (sectional design standard for flex circuit) dictate the acceptance criteria and design rules that help to ensure flex board reliability. These standards make material selection less guesswork and more of a repeatable and verifiable process.
JLCPCB's Flexible PCB Material and Manufacturing Capabilities
But while knowing the theory is one thing, putting it into practice requires a manufacturer that can provide the appropriate materials and ensure they are of consistent quality. That's where modern PCB manufacturers such as JLCPCB make it easy to choose flexible PCB material. JLCPCB uses polyimide base films to manufacture flex circuits and provides options that correspond closely to the above reliability principles, while also having inspection processes to detect problems in an early stage.
Flexible PCB Material Options for Different Applications
JLCPCB's flexible PCB service focuses on polyimide substrates, which are the most reliable and widely used material for soldered and high-reliability flex. The options available allow you to customize the build to your application.
- Standard thicknesses ideal for dynamic and static flex, on a polyimide base film.
- Coverlay and strain relief with pad openings defined.
- Weight choices for copper considering current capacity and flexibility.
- Surface finish such as ENIG for fine pitch, reliable solderability.
- Single and multilayer flex builds, ranging from simple connectors to complex interconnects.

Frequently Asked Questions (FAQ)
Q: What is the most common material used for flexible PCBs?
Ans: Polyimide (PI) is by far the most common base material for flexible PCBs. Its high thermal stability, excellent flex life, and solderability make it the default choice for soldered and high-reliability flex circuits.
Q: Can PET flexible PCBs be soldered like polyimide ones?
Ans: No, PET softens around 130-150°C and cannot survive standard reflow or wave soldering. PET-based flex circuits typically use conductive adhesives or crimped contacts to make connections instead.
Q: Why do flexible PCBs need to be baked before assembly?
Ans: Polyimide absorbs moisture from the air, and that trapped water can vaporize during reflow, causing delamination or popcorning. Pre-baking drives out the moisture and is a standard step for reliable flex assembly.
Q: What is a coverlay, and why does it matter for reliability?
Ans: A coverlay is a protective film, usually polyimide with adhesive, laminated over the traces — the flex equivalent of solder mask. It seals the traces from the environment and helps position copper near the neutral bending axis to reduce crack-causing strain.
Q: Which IPC standards apply to flexible PCB design and materials?
Ans: IPC-6013 covers the qualification and performance of flexible printed boards, while IPC-2223 defines the sectional design standard for flex circuits. Following both ensures your material choices and design rules meet recognized reliability criteria.

Popular Articles
• Choosing the Right Bend Radius for Durable Flexible PCBs
• Flexible Meets Durable: Understanding Rigid-Flex PCB Technology
• PCB Stiffeners: An Essential Requirement for Flexible Circuits
• The Ultimate Guide to Flexible PCB: Types, Design, and Applications
• 45 Must-Know Flex PCB Design Tips You Can't Afford to Miss!
Keep Learning
Choosing the Right Bend Radius for Durable Flexible PCBs
Key Takeaways Mastering the bend radius is essential for reliable flexible PCB design. Following IPC-2223 guidelines, maintain a minimum of 6× total thickness for static bends and 100× for dynamic applications, while using thinner RA copper, adhesiveless polyimide, staggered traces, and cross-hatched patterns in flex zones. Proper material selection, layer stackup optimization, and adequate clearance from stiffeners can dramatically extend flex life and prevent premature trace cracking or delamination......
Flex PCB Stackup Design Guide: Layers, Materials & Reliability
Key Takeaways A reliable flex PCB starts with the right stackup design. The layer structure, material selection, and copper arrangement directly affect flexibility, bend life, electrical performance, and manufacturing reliability. This guide explains single-sided, double-sided, and multilayer flex PCB stackups, including polyimide materials, coverlay, copper types, and key design considerations for creating durable flexible circuits with JLCPCB. Did you ever wonder how a foldable phone can last for 20......
Flexible Meets Durable: Understanding Rigid-Flex PCB Technology
In the rapidly evolving world of electronics, the demand for smaller, more reliable, and more versatile devices continues to grow. To meet these demands, engineers and designers are increasingly turning to Rigid-Flex PCBs. The circuit boards combine rigid and flexible substrates into a single interconnected structure. This combination allows for complex designs that can bend and flex in specific areas while maintaining rigidity in others. To manufacture rigid flex PCBs, IPC offers advice and best prac......
PCB Stiffeners: An Essential Requirement for Flexible Circuits
A printed circuit board stiffener plays an important role when it comes to offering mechanical support to a PCB. They are particularly helpful for flexible circuit boards, that given their name, are flexible and in need of stiffness in certain places. Stiffeners are particularly required when components are placed in a flex zone & the weight of these components stresses the flex material. These components provide a rigid connection from the flexible portion to the solid board. This solidity makes appl......
The Ultimate Guide to Flexible PCB: Types, Design, and Applications
Key Takeaways JLCPCB 1–4 Layer Flex PCB: Supports 1 to 4-layer FPCs with polyimide (PI) substrates and trace/space down to 3/3 mil. Stiffener Selection: Use PI (0.1–0.25mm) for ZIF connectors, FR4 (0.1–1.6mm) for SMT support, and Stainless Steel (0.1–0.3mm) for high rigidity. Layout Optimization: Use cross-hatched copper ground planes and stagger 2-layer traces to eliminate the "I-Beam effect." Surface & Protection: Combine Immersion Gold (ENIG 1u"/2u") for SMT planarity with flex coverlay to protect ......
Medical Flex Circuits: Manufacturing, Applications, Materials, and Design Guide
Medical flex circuits made to fit inside a 1.0 mm disposable endoscope, wrap around a hearing aid shell, and sit on a patient's arm for ten straight days. When one fails, it is not a warranty return but a device history file and a regulatory conversation. In this guide, you will learn: What separates a medical flex circuit from a consumer one How they are built, tested, and released Polyimide, copper, coverlay, and stiffener choices Fine line, bend radius, and layer count limits What to check before c......