This website requires JavaScript.
Coupons
Ship to
Help Center
Component Polarity & Orientation Identification Guide

Component Polarity & Orientation Identification Guide

Last updated on Sep 09, 2026

Table of Contents
  • Definition of Polarity
  • Common Polarized SMD Components

pcb prototype assembly banner 2

Definition of Polarity

Polarity refers to the correct alignment of a component’s positive/negative terminals or Pin 1 with the corresponding polarity markings or Pin 1 indication on the PCB (Printed Circuit Board). If the orientation of a component does not match the PCB markings, it is considered a reverse-polarity defect.

Throughout the PCBA process, polarity-related errors are critical. Incorrect orientation of polarized components may result in systematic failures, batch-level defects, or complete PCBA malfunction. Therefore, it is essential for engineering and production personnel to fully understand SMT component polarity rules. Polarity verification is also a key step in after-sales component failure analysis, to determine whether incorrect orientation caused PCBA failure or functional damage.

If you are using EasyEDA for PCB design or purchasing components through JLCPCB, polarity and orientation can often be quickly verified using the PCB footprint and schematic symbol libraries available on the JLCPCB / EasyEDA platform.

Common Polarized SMD Components

I. Capacitors

1. Tantalum Capacitors (Polarized Components)

On the physical component, the positive terminal is clearly marked. Common identification methods include:

  • Color stripe
  • “+” symbol
  • Chamfered (beveled) edge

When designing PCB pads and silkscreen, clear polarity markings must be included.

Tantalum capacitor

Tantalum capacitor PCB footprint

2. Aluminum Electrolytic Capacitors (Polarized Components)

a) SMD Type


For surface-mount electrolytic capacitors, the black band on the component body typically indicates the negative terminal.


Corresponding PCB footprint and silkscreen markings should reflect this polarity.

SMD aluminum electrolytic capacitorSMD aluminum electrolytic capacitor PCB footprint

b) Through-Hole Type


For through-hole electrolytic capacitors, the negative terminal is usually marked with a white stripe or a stripe of a different color than the rest of the body.

The PCB footprint and silkscreen should clearly indicate polarity

Through-hole aluminum electrolytic capacitor

II. Light-Emitting Diodes (LEDs) – Polarized Components

1. SMD LEDs

Polarity can be determined based on top-mount or bottom-mount orientation:

  • When viewed from the top, the side with a green marking typically indicates the cathode (negative terminal).
  • When viewed from the bottom, the arrow direction or raised arrow shape usually points to the cathode (negative terminal).

LED (Light-Emitting Diode) – top viewLED (Light-Emitting Diode) – bottom view

LED PCB footprint with polarity marking

2. Through-Hole LEDs

  • Before soldering, for two-lead LEDs, the longer lead is the anode (positive terminal).
  • After soldering, polarity can usually be identified by distinct markings on the LED body, such as a white stripe.

Through-hole diodeThrough-hole diode PCB footprint

III. Diodes – Polarized Components

For SMD diodes, the cathode (negative terminal) is typically indicated by:

  • A color band
  • A notch or groove

These markings should be visible on both the physical component and the PCB footprint.

SMD diodeSMD diode PCB footprint

IV. Integrated Circuits (ICs)

(Classification by Package Type)

IC polarity and orientation should be determined not only by the package marking, but also by cross-referencing the PCB silkscreen and pad layout.


During PCB design, it is essential to include clear silkscreen markings to enable unambiguous orientation verification.

It is generally recommended to place Pin 1 indicators outside the pad area or in an open board area for easy identification.

PCB footprint with polarity indicator

1. SOIC Packages

Pin 1 identification methods include:

  • Color stripe
  • Symbol marking
  • Dimple or notch
  • Chamfered edge

On the PCB footprint, Pin 1 is marked with a distinct and clear symbol near the corresponding pad.

SOIC package – polarity identification     SOIC package                                      

SOIC PCB footprint

2. QFP / SOP Packages

These are square or rectangular packages with leads on all four sides.

Pin 1 is typically identified by:

  • A dimple or notch
  • One dot that differs from other dots in size or shape

The PCB footprint includes a distinct Pin 1 indicator near the corresponding pad.

QFP / SOP package – polarity identification

QFP / SOP component and PCB footprint

3. QFN Packages

  • QFN packages with leads on two sides are typically rectangular.
  • QFN packages with leads on all four sides are typically square.

Common Pin 1 indicators include:

  • A dot that differs from other dots in size or shape
  • A chamfered corner
  • Symbol markings (e.g., line, “+” symbol, or dot)

The PCB footprint includes a clear and unique Pin 1 marking.

QFN package – polarity identification

QFN component and PCB footprint

4. BGA Packages

In classic BGA packages, such as CPUs, the underside of the package is populated with an array of solder balls.

Polarity / Pin 1 identification is typically indicated by:

  • Dimple or notch
  • Dot or circular marking

The PCB footprint includes distinct Pin 1 indicators.

BGA component and PCB footprint

V. Power Modules

Many power modules include polarity or orientation indicators.

For through-hole power modules, common indicators include:

  • Dimple or notch
  • Dot or circular marking

On the PCB footprint, polarity is typically indicated by a circular marking or a square pad.

Power module and PCB footprint

VI. Terminal Blocks / Connectors

Most terminal blocks do not have electrical polarity, but orientation during assembly is still critical, as it affects the alignment of external interfaces.

For these components, the footprint design typically includes directional indicators to ensure correct orientation during soldering and to avoid reversed connector installation.

Terminal block and PCB footprint

Final Notes:

When verifying component polarity and orientation, always combine PCB silkscreen markings with physical component markings for confirmation. This dual verification approach helps ensure correct polarity and orientation, minimizing the risk of functional failure or irreversible damage.