Questions about JLC3DP spray painting
Questions about JLC3DP spray painting
JLC3DP spray painting service is online, and the answers to related questions are as follows:
1) JLC3DP spray painting/spraying is artificial spraying, and the effect will have some flaws, which is a non-industrial grade effect.
2) Spray painting only sprays the outer surface of the model. If you have any requirements for the spray painting surface, please contact the customer service staff to communicate.
3) In order to unify the color number standard, JLC3DP spray painting uses Pantone color number C card (glossy) and U card (matte) as reference standards.
4) Due to the display problem of the electronic screen, there will be color differences between the actual object and the picture. Please refer to the actual object.
5) In order to improve the efficiency of spray painting, it is recommended to select the color number from the following 30 colors in the system. Other self-selected colors are not supported for the time being.
6) The estimated delivery time of the spray painting order is about 5 days. If you have any questions about the delivery time, please contact the salesperson in time for communication and confirmation.
7) The thickness of the paint surface is about 0.1MM-0.2MM.
8) A 0.15MM-0.2MM assembly gap needs to be reserved for the assembly of the assembled model, and the thickness of the paint surface needs to be reserved on the basis of the assembly gap for the assembly of the spray paint/spray oil model assembly.
9) Humid weather will cause slight whitening of the paint (matte black, matte silver), and it is recommended to use glossy black and glossy silver.
10) Matte paint surface is easy to scratch without protective coating, which is not suitable for small batches. It is recommended to use glossy surface. (Matte black is more serious).
Currently JLC3DP spray painting supports the following colors (C:glossy, U:matte) :
Black
white
Red
Vermilion
Light green
Green
Sky blue
Ultramarine
Yellow
Purple
Orange
Pink
Brown
Silver
Orange-yellow
The following is the physical comparison of JLC3DP glossy spray paint and matte spray paint:
Last updated on July 22, 2024