This website requires JavaScript.

How to Set the Temperature for Wave Soldering and What Are the Soldering Temperature Standards?

Blog  /  How to Set the Temperature for Wave Soldering and What Are the Soldering Temperature Standards?

How to Set the Temperature for Wave Soldering and What Are the Soldering Temperature Standards?

Oct 16, 2023

Wave soldering is a process used for soldering electronic components by inserting them into the holes on a Printed Circuit Board (PCB) and securing the components to the board using a molten solder wave generated by a wave soldering machine. Temperature is a crucial parameter during the wave soldering process, as it directly affects the quality and efficiency of soldering. Therefore, setting the temperature correctly for wave soldering is essential.


Temperature for Wave Soldering

Wave soldering machines typically employ radiant heating for preheating, with the most commonly used methods being forced hot air convection, electric hotplate convection, electric heating rods, and infrared heating. Among these methods, forced hot air convection is generally considered the most effective method for heat transfer in most processes. After preheating, the PCB is soldered with either a single wave (λ wave) or dual waves (turbulent wave and λ wave). For through-hole components, a single wave is usually sufficient. When the PCB enters the wave, the direction of solder flow is opposite to the board's movement, creating eddies around component pins. This acts like a washing action, removing residues of flux and oxide films and forming proper wetting as the solder reaches its wetting temperature.

Factors

Setting the temperature for wave soldering involves considering multiple factors, including the solder's melting point, the material of the PCB, and the type of components being soldered. Generally, the temperature for wave soldering should be set near the melting point of the solder and slightly higher to ensure complete melting and good wetting on the soldering surface. However, the temperature should not be too high to avoid damage to the PCB and components.

Usually, the temperature setting for wave soldering needs to be adjusted based on the type of solder used and specific equipment parameters. When adjusting the temperature, it's advisable to gradually increase the temperature while continuously observing the color changes on the soldering surface and recording the temperature variations. In general, the temperature of the soldering surface should fall within the range of 240°C to 260°C, with a maximum temperature not exceeding 280°C.

In addition to temperature, the soldering time is also a critical factor affecting soldering quality. Too short a soldering time can result in incomplete soldering, while excessive time may damage components. Therefore, adjustments should be made according to specific circumstances to achieve the optimal soldering effect.



To sum up, setting the temperature for wave soldering involves considering various factors, including the type of solder, PCB material, and component types. When adjusting the temperature, it's important to gradually increase it while monitoring the color changes on the soldering surface and recording temperature variations to achieve the best soldering results.


Soldering Temperature Standards

Soldering temperature standards refer to the temperature range that should be achieved during the soldering process. For wave soldering, the soldering temperature standard typically falls in the range of 240°C to 260°C. Within this temperature range, the solder, when molten, can flow adequately and wet the soldering surface properly, resulting in stable solder joints.

In addition to the temperature range, soldering temperature standards also need to consider other environmental factors such as humidity and airflow. High humidity and airflow can impact soldering effectiveness. Therefore, adjustments should be made based on the specific production environment to ensure soldering quality and efficiency.


Conclusion

In summary, soldering temperature standards are of paramount importance for the quality and efficiency of wave soldering. Adjustments should be made based on the specific production conditions and environment to ensure soldering quality and efficiency. Regular maintenance and upkeep of wave soldering equipment are also essential to maintain stability and production efficiency. Wave soldering has a history dating back to 1956 when the British company Fry's Metal introduced the concept of printed circuit board wave soldering. It revolutionized the soldering process from manual soldering with soldering irons to automated, large-scale, and highly efficient soldering by machines. Wave soldering offers advantages such as speed, accuracy, and efficiency. It has made significant contributions to reducing soldering defects, improving the reliability of electronic products, lowering production costs, reducing the labor intensity of workers, and increasing production efficiency.


GET FREE QUOTE>>

Recent Posts