What Is CAM: Computer-Aided Manufacturing Basics
5 min
- What Is CAM?
- How Does CAM Work?
- CAM in Electronics and PCB Manufacturing
- CAM Software Tools:
- CAM vs CAD: What's the Difference?
- Benefits of CAM in Electronics Manufacturing:
- Conclusion:
When electronics start evolving, the circuits start becoming more complex and integrated. Before, these circuits were made using hand-drawn paper, but the evolution of digital electronics changed the perspective. Nowadays, we have CAD (Computer-Aided Design), which has become the art of creating a blueprint. Just define the functionality of a circuit, and we can nowadays easily synthesise a circuit only in software. The software has become so advanced that the whole digital flow is possible without looking into the actual circuit, but only by programming.
Evolution is not only for design but also for manufacturing. As the technology becomes more advanced, we need advanced manufacturing tools to fulfil the requirements. This is only possible due to the involvement of computers. And that’s where CAM, or Computer-Aided Manufacturing, comes into play. CAM is nothing but the process of converting the blueprint design into reality. Machines nowadays can be handled without any manpower; moreover, all the machines work automatically, which increases efficiency and productivity. In this article, we'll explain what CAM is, how it works, its role in electronics and PCB production, and the advantages it offers to modern engineering.
What Is CAM?
Computer-Aided Manufacturing (CAM) refers to the use of computer software and systems to plan, control, and automate manufacturing processes. This means that nowadays computers are not only focused on software but have a great command of hardware. We can integrate software to run the corresponding hardware, which turns the machines into automatic CAM models.
- CAM bridges the gap between design (CAD) and physical production.
- It translates digital models into machine instructions for CNC machines, PCB fabrication tools, and 3D printers.
- CAM software ensures that design files (Gerber, drill, netlists) are interpreted correctly for fabrication.
How Does CAM Work?
The CAM workflow generally follows these steps:
1. Import Design Files: CAM software imports CAD files such as Gerber files for PCBs and STEP files for mechanical parts.
2. Process and Optimize: The software checks design data against manufacturing rules. DFM is one of the main CAM tools used in the PCB industry. It is used for flagging errors, such as missing pads, overlapping traces, or incorrect drill sizes.
3. Toolpath Generation: After this, the CAM creates toolpaths, which are the precise instructions that machines follow. For PCBs, the software includes paths for drilling, etching copper, and milling board outlines.
4. Simulation: Before manufacturing the goods, as per requirements, it always performs virtual runs and simulations, through which engineers verify correctness before physical material is wasted.
5. Manufacturing Execution: The final output of the software is a machine-readable code, for example - the G-code. The machine code is then executed by PCB assembly machines, such as laser cutters and pick-and-place machine.
CAM in Electronics and PCB Manufacturing
1. PCB Fabrication: Gerber and Excellon files come as the main input from the users, which are then processed by CAM software. CAM checks trace widths, clearances, drill sizes, and solder mask alignment. One of the best examples of CAM is the DFM software by JLCPCB. After that, some adjustments are made for manufacturing tolerances.
2. PCB Assembly (PCBA): BOM and CPL files are the main input for the assembly; the CAM drives pick-and-place machines, which place SMD components according to the BOM. Usually, the pick and place machine is fed manually using the components of the BOM.
3. CNC Machining for Electronics Enclosures: For housings and heatsinks, CAM generates CNC toolpaths, which are then fed into the CNC or 3D printing memory to perform the actions as per the given co-ordinates.
CAM Software Tools:
Some widely used CAM software in electronics and PCB manufacturing:
- CAM350: Specialized for PCB Gerber analysis and verification.
- Altium CAM Editor: Built-in for PCB manufacturing output.
- KiCad Plot & CAM Tools: Open-source PCB CAM export.
- Fusion 360 (Autodesk): General-purpose CAD/CAM with PCB mechanical support.
- Mastercam / SolidCAM: Popular in CNC and mechanical parts manufacturing.
CAM vs CAD: What's the Difference?
Benefits of CAM in Electronics Manufacturing:
Accuracy and Precision: Reduces human errors in interpreting CAD files. It also ensures the tight tolerances as per high-speed PCB designs.
Efficiency and Speed: Automation reduces manual programming of machines. Also speeds up PCB prototyping and large-scale production.
Consistency and Repeatability: Every board or part that comes out is manufactured using the same code and is identical, which is essential for mass production and quality control.
Cost Reduction: Overall, less material is wasted due to pre-simulation and toolpath optimization, aollowing early error detection. This avoids costly production failures.
Conclusion:
Computer-Aided Manufacturing is the digital bridge between design and production. In the software, we can join wires in schematics and then make the layout for it in another tool, but at the machine end, it is nothing but the coordinated commands known as machine codes. These machine codes are widely utilized in every sector of PCB manufacturing, and the CAM software is the one that makes the machine codes out of CAD. This is just the beginning; the future is quite big for CAM, from AI-assisted to cloud and integration of multiple tools. Understanding CAM is important to operate the machines. We have discussed the complete workflow through which you can get a basic understanding. For more information, you can visit the JLCPCB blog section.
Keep Learning
Technical Guidance: Mouse Bite Panelization Guide
The conventional method of panelization uses V-grooves. However, for irregularly-shaped boards or special requirements (such as JLCPCB's economic SMT assembly), mouse bite panelization, which resembles postage stamps on an envelope, is required. PCBs panelized using this method are called "mouse bite panels" or "mouse bite connections". Mouse bite panelization can be referred to as "universal panelization." As long as there is a position to add mouse bites, boards of various shapes can be interconnect......
Technical Guidance: V-Cut Panelization Standards
For boards with regular rectangular shapes, V-cut (V-scoring) panelization is an efficient method. This process involves cutting V-shaped grooves of a specific depth on both sides of the panel along the board boundaries, leaving a thin web of material (typically about 1/3 of the board thickness) that allows easy manual separation after SMT assembly. After separation, minor thread-like fibers or rough edges may remain and can be lightly scraped off. Due to material expansion and cracking during depanel......
How Laser-Made PCBs Are Used in Rapid Prototyping
Key Takeaways Speed & Precision: Digital lasers enable 24-hour quick-turn HDI and FPC prototyping without mechanical tooling. LDI Patterning: Replaces physical photo-films to deliver precise circuit traces down to 2/2 mil. HDI Microvias: UV/CO2 lasers drill 0.075–0.15 mm blind vias (1:1 aspect ratio) for 1+N+1 to 3+N+3 stackups. Laser Profiling & Stencils: Achieves ±0.05 mm FPC cut accuracy and ±0.003 mm LPKF stencil aperture precision. Laser DFM: Maintain ≥ 0.30 mm copper clearance on FPCs and ≥ 0.07......
A Beginners Guide to Tented vs Untented Vias
Via’s are important, If working at high speed design and HDI boards then they become super important. Choosing a type of via during PCB manufacturing matters. Via’s are basically joining two or more layer traces together. Shape, size and track length guidelines became more interesting at high frequency and high speed signals. Today in this article we will explore a fabrication side, the decision to use tented or untented vias. This beginner-friendly guide explains what tented vias are, the differences......
Flex PCB Fabrication: Process, Materials, Design Rules & Cost
Many of the basic steps in rigid PCB fabrication also apply to flexible PCB fabrication. However, it is made with thin polyimide or PET films that can swell or shrink during processing due to moisture and temperature changes. These material attributes bring further complexities to considerations of layer alignment, coverlay openings, and bend-zone design. For instance, if there's not enough room for adhesive flow in a coverlay opening, or if a via falls in a bend zone, manufacturing defects or assembl......
Smart PCB Array Design for Higher Yield and Lower Production Costs
Key Takeaways Smart PCB array design is a critical strategy for achieving higher manufacturing yield and significantly lower production costs. By optimizing panelization with proper board spacing, V-scoring, tab routing, and mouse bites, designers can dramatically improve material utilization by 20-30%, enhance production throughput, and simplify handling and depaneling while minimizing mechanical stress and defects. Effective use of fiducials and careful component clearance further ensures high-quali......