How to Read Resistor Color Code: Complete Guide with Chart and Examples
6 min
- 4-Band Resistor Color Code Explained
- 5-Band Resistor Color Code Explained
- 6-Band Resistor Color Code Explained
- Common Mistakes When Reading Resistor Color Codes
- FAQ
4-Band Resistor Color Code Explained

A 4-band resistor color code is one of the most common methods used to indicate resistance values in electronic components. It is widely used to help engineers and hobbyists quickly determine resistance values without using a resistor color code calculator.
In a standard 4-band resistor:
- First Band (Digit 1): Represents the first significant digit
- Second Band (Digit 2): Represents the second significant digit
- Third Band (Multiplier): Indicates the factor by which the first two digits are multiplied
- Fourth Band (Tolerance): Specifies the allowable deviation from the nominal resistance value
How to Read a 4-Band Resistor Color Code
Preparation: Hold the resistor so the band with the largest gap (or the gold/silver band) is on the right. Read from left to right.
- First & Second Bands (Digits): Match the colors to the chart to get the first two numbers.
- Third Band (Multiplier): This tells you how many zeros to add to the first two digits.
- Fourth Band (Tolerance): This represents the precision of the resistor (e.g., Gold = ±5%).
Example: 1kΩ Resistor (4-Band)
This is one of the most commonly used resistors, often found in pull-up circuits and basic LED applications.
- 1st Band: Brown (1)
- 2nd Band: Black (0)
- Multiplier: Red (×100)
- Tolerance: Gold (±5%)
Calculation:
10 × 100 = 1,000Ω (1kΩ)
5-Band Resistor Color Code Explained

A 5-band resistor color code is typically used for high-precision resistors. Compared to a 4 band resistor color code, the 5-band version provides higher accuracy by including an additional significant digit.
In a standard 5-band resistor:
- First Band (Digit 1): First significant digit
- Second Band (Digit 2): Second significant digit
- Third Band (Digit 3): Third significant digit
- Fourth Band (Multiplier): Multiplies the three-digit value
- Fifth Band (Tolerance): Indicates the allowable deviation from the nominal resistance
How to Read a 5-Band Resistor Color Code
Preparation: To find the first band, look for the side where the color bands are closer together. The larger gap or the wider band should be on your right (this is the tolerance).
Follow these steps from left to right:
- First 3 Bands (Digits): Read the first three colors as the three significant digits of the resistance value.
- 4th Band (Multiplier): Multiply the first three digits by the value of this band (usually represented by the number of zeros).
- 5th Band (Tolerance): This band indicates the precision of the resistor (e.g., Brown = ±1%).
Example: 4.7kΩ Precision Resistor (5-Band)
- 1st Band: Yellow (4)
- 2nd Band: Violet (7)
- 3rd Band: Black (0)
- Multiplier: Brown (×10)
- Tolerance: Brown (±1%)
Calculation:
470 × 10 = 4,700Ω (4.7kΩ)
6-Band Resistor Color Code Explained

A 6 band resistor color code is used for high-precision resistors, adding an extra band to indicate the temperature coefficient, which describes how the resistance value changes with temperature.
In a standard 6-band resistor:
- First Band (Digit 1): First significant digit
- Second Band (Digit 2): Second significant digit
- Third Band (Digit 3): Third significant digit
- Fourth Band (Multiplier): Multiplies the three-digit value
- Fifth Band (Tolerance): Indicates the allowable deviation from the nominal resistance
- Sixth Band (Temperature Coefficient): Specifies how resistance changes with temperature (ppm/°C)
How to Read a 6-Band Resistor Color Code
Preparation:
To orient the resistor correctly, look for a larger gap between the 5th and 6th bands. This gap indicates that the 6th band is the Temperature Coefficient and should be on the right.
To read a 6-band resistor color code, follow these steps: (Read from Left to Right):
- First 3 Bands (Digits): Identify the first three colors to determine the three significant digits.
- 4th Band (Multiplier): Multiply the digits by this value (e.g., Orange = × 1,000).
- 5th Band (Tolerance): Indicates the precision (e.g., Brown = ±1%).
- 6th Band (Temperature Coefficient): Represents how much the resistance changes with temperature, expressed in ppm/°C (parts per million per degree Celsius).
Example: 10kΩ High-Precision Resistor (6-Band)
Common in temperature-sensitive and high-reliability applications such as medical and aerospace systems.
- 1st–3rd Bands: Brown (1), Black (0), Black (0) → 100
- Multiplier: Red (×100)
- Tolerance: Brown (±1%)
- Temp. Coefficient: Blue (10 ppm/°C)
Calculation:
100 × 100 = 10,000Ω (10kΩ)
Common Mistakes When Reading Resistor Color Codes
1. Reading the Resistor Backwards
One of the most frequent mistakes is starting from the wrong end.
Tip: Always identify the tolerance band first (gold/silver) and read from the opposite side.
2. Confusing Similar Colors
Colors like:
- Red vs Orange
- Brown vs Red
- Blue vs Violet
can look similar under poor lighting.
Tip: Use a reference chart or digital tool when in doubt.
3. Miscounting the Number of Bands
Confusing a 5-band resistor with a 4-band one can lead to 10× or 100× errors.
Tip: Always count carefully before decoding.
4. Ignoring the Multiplier Band
Some users correctly read the digits but forget to apply the multiplier.
Tip: This results in completely incorrect resistance values.
5. Assuming All Resistors Use Color Codes
Not all resistors use color bands.
- SMD resistors use numeric codes
- Zero-ohm resistors may not follow standard rules
Tip: Always identify the resistor type first.
6. Overlooking Tolerance
Tolerance affects circuit performance, especially in precision applications.
Tip: A 1kΩ resistor with ±5% tolerance can range from 950Ω to 1050Ω
FAQ
Q: What Is a "Reliability" Band on a Resistor?
In a 6-band resistor color code, the sixth band is known as the reliability band. It indicates the resistor’s failure rate, typically expressed as a percentage per 1,000 hours of operation. Not present in standard 4-band or 5-band resistors. This band is mainly used in high-reliability applications, such as aerospace, and industrial electronics, where long-term performance is critical. Rarely used in consumer electronics.
Q: How Do You Identify and Read SMD Resistor Codes?
SMD resistors (surface mount resistors) are typically small, black rectangular components without color bands. Instead of color coding, they use 3-digit, 4-digit, or alphanumeric markings to represent resistance values. Learn how to decode them step by step here: An Ultimate Guide to Read SMD Resistor Codes
Q: What Is a Zero-Ohm Resistor?
A zero-ohm resistor is a resistor with approximately 0Ω resistance, used primarily as a jumper or bridge on a PCB rather than for limiting current.
Although they are called “resistors,” their main function is to act as a low-cost, surface-mountable connection. Unlike standard resistors, zero-ohm resistors may use a single black band or be marked with “0” or “000” (in SMD form) and do not follow standard resistor color code rules. Zero-ohm resistors are commonly used for circuit routing and configuration, PCB design flexibility and automated assembly instead of wire jumpers.
Popular Articles
• How to Design and Assemble a Reliable ESP32 Module PCB on a 2-Layer Board
• The Ultimate Guide to PCBA: Process,Types and Techniques for the Electronics Enthusiast
• How to Create a Bluetooth-Controlled Car With Arduino: A Step-by-Step Guide
• Logic Gate Symbols: The Complete Chart, Truth Tables [2026]
• The Ultimate Guide to Relay Symbol: Coil, Contacts, Diagrams, and Circuit Applications
Keep Learning
How to Design and Assemble a Reliable ESP32 Module PCB on a 2-Layer Board
Many engineers fail when designing their first ESP32 PCB due to antenna issues, power instability, or SMT defects. Designing a custom board with an ESP32 Module strikes the perfect balance between customizability and ease of manufacturing. Unlike a chip-down design, the module integrates the crystal oscillator, flash memory, and RF matching network, reducing the PCBA risk significantly. the SMD package (for example, ESP32-S2-WROOM modules) introduces several assembly considerations, including pad sold......
Solder Paste vs Flux: What's the Difference and When Should You Use Each?
Solder paste and flux are not interchangeable. Solder paste contains solder alloy powder and flux, while flux contains no solder alloy. This difference matters when choosing materials for SMT, reflow soldering, or manual soldering. Flux removes metal oxides and prevents re-oxidation, allowing molten solder to wet copper pads and component leads properly. Solder paste combines flux with fine solder alloy powder. During reflow, the flux activates to improve wetting while the solder alloy melts to form t......
The Ultimate Guide to PCBA: Process,Types and Techniques for the Electronics Enthusiast
As the demand for electronic devices continues to grow, understanding the complexities of Printed Circuit Board Assembly (PCBA) has become increasingly crucial. This comprehensive guide will provide an in-depth look at the PCBA process, the types of PCB assembly, and the various techniques and tips involved. We will also explore the meaning of PCBA in electronics, ensuring you have a thorough understanding of this vital component. What does PCBA stand for in Electronics? PCBA stands for Printed Circui......
How to Create a Bluetooth-Controlled Car With Arduino: A Step-by-Step Guide
This tutorial walks through the complete engineering and implementation of a two-wheel Bluetooth RC car with an Arduino Nano module on a specially designed PCBA (Printed Circuit Board Assembly). While many hobbyists start by wiring motors and Bluetooth modules with jumper cables on a breadboard, this approach is prone to disconnection and signal noise. This guide upgrades that process by teaching you how to design a professional mainboard. Key Design Features Controller: Arduino Nano used as a plug-in......
Potentiometer Symbol Guide: Complete Chart, IEC/IEEE Standards, Compare Types and More
Key Takeaways ⬇ Download the Potentiometer Symbol Cheat Sheet (PDF) Find the wiper first: The arrow or bar that touches the resistor body is the wiper, the movable contact, while the two plain leads at the ends of the body are the fixed end terminals. Expect two drawing styles: IEC schematics draw the body as a rectangle, and ANSI-style schematics draw a zigzag, but both represent the same component and mark the wiper in the same way. Read the arrow's position: An arrow touching the body marks a three......
Logic Gate Symbols: The Complete Chart, Truth Tables [2026]
Note ⬇ Free Download: Logic Gate Symbols PDF Reference Chart Save time when working with digital schematics. This downloadable Logic Gate Symbols PDF includes all basic logic gates, standard symbols, truth tables, Boolean expressions, and common 74xx/4000-series IC references — a practical reference for students, engineers, and PCB designers. When we define digital logic on a schematic, we use logic gate symbols to represent Boolean operations and show how signals are processed in a circuit. A single ......