How Inner Layer Residual Copper Rate Affects PCB Thickness and Quality
4 min
- How Inner Layer Copper Affects Board Thickness
- Importance of Residual Copper Rate
- The Role of PP Sheets in Multilayer Lamination
- Consequences of Low Residual Copper Rate
- JLCPCB Recommendations
- Common Issues in Gold Finger Design
- Common Issues in PCB Gold Finger Design
In printed circuit board (PCB) manufacturing, precision is crucial for maintaining quality and performance. One key factor that significantly influences PCB quality is the residual copper rate in the inner layers. This concept becomes particularly critical in multilayer PCBs, where the balance of copper distribution impacts the final board thickness. This article explores how the inner layer residual copper rate affects board thickness and the importance of optimizing this rate to ensure robust and reliable PCBs.
How Inner Layer Copper Affects Board Thickness
As shown in the diagram, when the copper coverage in the inner layer is minimal, the (PP prepreg) sheets, regardless of their thickness, must spread evenly to fill the gaps between layers. Once the PP sheets cool and solidify, the reduced resin volume leads to a thinner overall board thickness.
Importance of Residual Copper Rate
So, how much copper should be laid in the inner layer to ensure that the board thickness doesn’t fall below tolerance limits? This is where the "residual copper rate" comes in. The residual copper rate refers to the percentage of the inner layer's copper circuit patterns relative to the entire surface area of the board.
Residual copper rate = the area of copper in the current layer / total area of the board.
The Role of PP Sheets in Multilayer Lamination
In multilayer board lamination, PP sheets are cut into pieces and placed between the inner core board and another core board, or between the core board and copper foil. The resin on the PP melts under high temperature and pressure, filling the copper-free areas on the core board. After cooling, the resin solidifies, bonding the core board and copper foil together.
Consequences of Low Residual Copper Rate
If the residual copper rate is too low, the overall board thickness decreases, and uneven copper distribution across layers can lead to board warping.
This is especially critical for boards with gold fingers, as their thickness must be precise to ensure a proper fit in slots. A thinner board may result in a loose fit or poor contact when inserted into the slot.
JLCPCB Recommendations
JLCPCB enginners strongly recommend :
1. For Gold Finger Multilayer Boards
Cover the blank areas with copper, especially in the inner layers near the gold finger region. This prevents issues such as the board being too thin to fit into the slot or variations in line widths.
2. For Residual Copper Rates Below 25%
To minimize uneven electroplating, which can cause inconsistent line widths and excessive board thickness deviations, add copper to the blank areas.
Common Issues in Gold Finger Design
For the golden finger areas in both the inner and outer layers, ensure that there is an open window (i.e., no solder mask bridge between each golden finger pad) to prevent frequent insertion and removal from causing ink to fall into the golden finger slot, which can result in poor contact and other functional issues.
For all types of PCBs, add copper to blank areas whenever possible, as long as it does not affect the board's performance. For boards with a residual copper rate below 25%, ensure that copper is added. In gold finger boards, copper should be applied to the inner layer near the gold finger area, and the outer layer should have a solder mask with a properly open window in the gold finger area.
Common Issues in PCB Gold Finger Design
For the golden finger areas in both the inner and outer layers, ensure that there is an open window (i.e., no solder mask bridge between each golden finger pad) to prevent frequent insertion and removal from causing ink to fall into the golden finger slot, which can result in poor contact and other functional issues.
For all types of PCBs, add copper to blank areas whenever possible, as long as it does not affect the board's performance. For boards with a residual copper rate below 25%, ensure that copper is added. In gold finger boards, copper should be applied to the inner layer near the gold finger area, and the outer layer should have a solder mask with a properly open window in the gold finger area.
Keep Learning
Microstrip Line Design Techniques for High-Speed PCB Excellence
Have you ever routed a high-speed signal on an outer routing on your PCB and wondered whether the geometry of the traces you selected would actually work at multi-gigabit data rates? You’re definitely not alone. The most commonly used transmission line structure in PCB design is the microstrip line, but this line is immensely geometry-sensitive, material-sensitive, and manufacturer-tolerance-sensitive. The difference between a clean eye diagram and a signal-integrity nightmare is whether the microstri......
Mastering Mitered Corners for Superior High-Speed Signal Performance
Have you ever had the privilege of zooming into a PCB layout and noted those well-chamfered corners on high-speed signal traces? Mitered corners they are, and much more than a cosmetic preference. The geometry of each trace bend is directly proportional to impedance continuity, signal reflection, and the quality of your data being transmitted at the RF and high-speed digital frequencies. Having mitered corners on your PCB can be the difference between meeting your return loss target and trying to trac......
How Design Rule Check Prevents Expensive PCB Production Mistakes
Have you ever sent Gerber files to your fab house, and you can get an email back saying that they need to fix clearance or annular ring issues, and only then can they start production? When that comes out like you, you know how frustrating that can be, days wasted, revision numbers rising, shipping dates falling. Catching all of that is actually the real MVP of good design, which is a solid design rule check in your PCB layout tool, that allows you to discover all of that before it even leaves your de......
Why Sequential Lamination Delivers Superior HDI PCBs
Did you ever ask yourself how smartphone manufacturers can crust a thousand connections into a credit card-sized board? The process is referred to as sequential lamination, which is a multi-cycle process that is used to fabricate PCBs on a layer-by-layer basis, releasing microvia structures and routing densities that cannot be accessed by a single-press process. Without it, the slick, high-performance electronics that we all use on a daily basis would not appear the way that they do now. With data rat......
The Foundation of Every Great PCB: Mastering Schematic Capture
Schematic capture is the process of creating an electronic circuit diagram using specialized software. Here we have to place component symbols (such as resistors, capacitors, ICs, and connectors) and connect them with wires to represent the electrical connection. Although it is not the real connection yet, but can be translated once it goes to layout. Hence, we can say on a big scale schematic capturing serves as the first step in the PCB design workflow, which allows designers to define how component......
Halogen Free PCB: The Smart Choice for Safe, RoHS-Compliant, and High-Performance Boards
Engineers designing today’s electronics face a clear choice: continue using traditional FR-4 with halogenated flame retardants or switch to Halogen Free PCB materials that meet strict environmental and safety standards while delivering comparable or better performance. Halogen Free PCBs replace bromine and chlorine with phosphorus- or nitrogen-based retardants, significantly reducing toxic smoke and corrosive gases during combustion. This makes them the preferred option for consumer electronics, autom......