Preventing PCB Warping: Best Practices for Design and Manufacturing
Preventing PCB Warping: Best Practices for Design and Manufacturing
In the design and manufacturing process of electronic equipment, PCB (Printed Circuit Board) warpage is a common but troublesome problem. PCB warping not only affects the performance and reliability of the device but can also cause connectivity issues and other serious consequences. Therefore, it is crucial to understand how to prevent and resolve PCB warping. This article will explore some best practices in design and manufacturing to help you effectively prevent PCB warpage problems from occurring.
What is PCB warpage?
PCB warpage refers to the bending of the circuit board. It refers to the fact that the two ends or the middle of the originally flat circuit board are slightly tilted upward when placed on the table.
In actual production, most PCBs will have some degree of bend rather than being completely flat. How can the warpage standard of a PCB be measured? The degree of warpage of a PCB is typically evaluated by measuring its "warpage."
According to IPC standards, the permissible warpage for a PCB board with surface mount components is 0.75%, whereas for a PCB board without surface mount components, it is 1.5%. However, in order to meet the demands of high-precision and high-speed placement, some electronic assembly manufacturers have stricter requirements for warpage. Some requirements allow for 0.5% warpage, and a few even require 0.3%.
The Dangers of PCB Warping
It hinders the installation of SMT electronic components, leading to poor contact between the components (including integrated chips) and the solder joints of the PCB board.
It increases the difficulty of mounting electronic components and makes it difficult to cut off the pins.
During the wave soldering process, some pads may not effectively connect to the solder surface due to warping.
These problems not only affect production efficiency but may also lead to equipment performance degradation and reliability issues. Therefore, it is crucial to prevent and solve PCB warpage to ensure the stability and reliability of electronic devices.
Causes of PCB Warping
Deformation caused by the weight of the circuit board.
The weight of the circuit board causes it to dent and deform. In the reflow oven, the two sides of the board act as fulcrums to support the entire board. If there are heavy objects on the board or if the size is too large, it will cause the board to dent in the middle, leading to bending.
The Effect of V-Cut on Panel Deformation
The V-cut is a significant factor in compromising the structure of the board as it creates grooves in the original large piece of board, making deformation more likely at the V-cut.
Warpage caused by the PCB pressing process
Mainly results from thermal stress, increased thickness, varied pattern distribution, more prepregs, and challenges in eliminating thermal stress.
Improper Storage
Stacking boards or inadequate shelf support during storage can result in mechanical deformation, especially for thin boards.
The copper surface area is uneven
With more on one side and less on the other, resulting in uneven surface tension and excessive temperature causing the board to warp.
How to Prevent Circuit Board Warping
● Optimized design:
Ensure that the design complies with standard size and weight requirements and avoid excessively large or heavy designs.
Reasonably arrange the V-Cut design to reduce damage to the board structure.
● Material Selection:
Use a high-quality PCB substrate, such as fiberglass-reinforced FR-4, to reduce the possibility of warping. Consider choosing a thinner substrate, as thicker substrates can easily cause warping.
● Proper storage:
During the storage of semi-finished products, it is important to avoid stacking and improper storage of panels, especially thin ones.
● Uniform distribution of copper foil:
Evenly distribute copper foil on both sides of the PCB to ensure consistent heat conduction and material performance.
Solution to Circuit Board Soldering Warping
1. Control temperature: During the welding process, it is important to maintain uniform temperature in different areas. This can be achieved by adjusting the welding temperature or changing the welding method. During welding, it is essential for the solder to be fully wetted to prevent the formation of bubbles and gaps between the welds.
2. Optimize the structure: The structural design of the circuit board will also impact soldering warpage. Therefore, we can reduce the thermal disturbance during the welding process and minimize the warpage of the circuit board by modifying the circuit board structure and adjusting the position of the solder joints.
3. Reinforce the circuit board: To address soldered warps on circuit boards, reinforcement can be applied as a solution. For example, support can be reinforced in areas where the circuit board is severely warped, or solder joints can be added in the warped areas.
4. Replace the material: If none of the above measures are effective, consider replacing the material. Choosing materials with lower thermal expansion coefficients or implementing surface bonding technology can help minimize circuit board solder warpage.
Recent Posts
• Understanding and Utilizing Breakout Boards in Electronics Projects.
June 29, 2024
• Comparing HASL and ENIG Surface Finishes for PCBs
June 29, 2024
• Future Trends and Innovations in Flex PCB Technology
June 28, 2024
• Using Via-in-Pad Technology: What You Need to Know, Design Guidelines, and More…
June 27, 2024
• Flex PCB Designing Useful Tips - JLCPCB
June 25, 2024