How to Easily Distinguish Between Adhesive-Based and Adhesive-Free FPC Substrates
3 min
- 1. Structure of Adhesive-Based and Adhesive-Free Substrates
- 2. Differences Between Adhesive-Based and Adhesive-Free Substrates
- 3. How to Identify Adhesive-Based and Adhesive-Free Substrates
FPC substrate is crucial to the performance of flexible circuit boards! It directly affects the reliability and lifespan of your product.
Currently, the most commonly used FPC substrate (also known as FCCL) on the market is Polyimide (PI), which has excellent heat resistance, chemical stability, and mechanical properties, allowing it to maintain stable insulation performance in high-temperature environments.
However, please note that PI substrates are categorized into adhesive-based and adhesive-free types, each with significant differences in material composition, performance, and application.
Currently, all JLCPCB FPCs use adhesive-free substrates, except for transparent PET materials. Below, we explain the differences and how to identify FPC substrates.
1. Structure of Adhesive-Based and Adhesive-Free Substrates
Adhesive-Based Substrate: Mainly consists of a three-layer structure: PI film/adhesive (AD)/copper foil. It is made by coating, pressing, and baking. The adhesive is typically epoxy resin or acrylic adhesive.
Adhesive-Free Substrate: Composed of PI film and copper foil. There are two production methods:
One method is laminating PI film with copper foil through hot pressing. This type of PI requires special treatment and is also called TPI, which is considered a trade secret. JLCPCB FPC substrates use this technology.
The other method is applying liquid PI onto the copper foil.
2. Differences Between Adhesive-Based and Adhesive-Free Substrates
Since adhesive-free substrates do not require adhesive as a bonding agent, their performance is superior to adhesive-based substrates. Currently, 90% of products on the market require adhesive-free substrates, with the specific differences listed below:
3. How to Identify Adhesive-Based and Adhesive-Free Substrates
Although most products in the market require adhesive-free substrates, many manufacturers use inferior materials to cut costs, passing off adhesive-based substrates as adhesive-free. Below are two quick identification techniques:
1. Check the Thickness
Standard FPC substrate PI thickness is 25um, while extra-thick FPC PI thickness is 50um. Copper thickness options: 12um, 18um, 35um. Coverlay thickness options: 27.5um and 50um (white coverlay requires an additional 10um).
Formula for finished board thickness: Copper thickness + Substrate + Coverlay = Finished Board Thickness
If the actual measured FPC thickness deviates significantly from the calculated thickness, it is likely using an adhesive-based substrate. Example: For a standard FPC double-sided board with 12um copper, the structure is as follows:
From above picture ,total calculated thickness = 0.104mm . If the actual measured board thickness is 0.13mm, then it is likely an adhesive-based substrate.
2. Cross-Section Analysis
Cut a cross-section of the FPC and observe it under a microscope. Check whether there is AD adhesive between the PI and copper layers. This method provides a more accurate judgment of whether the board uses an adhesive-based substrate.
How is it? Did you learn it?
Popular Articles
• Choosing the Right Bend Radius for Durable Flexible PCBs
• Flexible Meets Durable: Understanding Rigid-Flex PCB Technology
• PCB Stiffeners: An Essential Requirement for Flexible Circuits
• The Ultimate Guide to Flexible PCB: Types, Design, and Applications
• 45 Must-Know Flex PCB Design Tips You Can't Afford to Miss!
Keep Learning
Choosing the Right Bend Radius for Durable Flexible PCBs
Key Takeaways Mastering the bend radius is essential for reliable flexible PCB design. Following IPC-2223 guidelines, maintain a minimum of 6× total thickness for static bends and 100× for dynamic applications, while using thinner RA copper, adhesiveless polyimide, staggered traces, and cross-hatched patterns in flex zones. Proper material selection, layer stackup optimization, and adequate clearance from stiffeners can dramatically extend flex life and prevent premature trace cracking or delamination......
Flex PCB Stackup Design Guide: Layers, Materials & Reliability
Key Takeaways A reliable flex PCB starts with the right stackup design. The layer structure, material selection, and copper arrangement directly affect flexibility, bend life, electrical performance, and manufacturing reliability. This guide explains single-sided, double-sided, and multilayer flex PCB stackups, including polyimide materials, coverlay, copper types, and key design considerations for creating durable flexible circuits with JLCPCB. Did you ever wonder how a foldable phone can last for 20......
Flexible Meets Durable: Understanding Rigid-Flex PCB Technology
In the rapidly evolving world of electronics, the demand for smaller, more reliable, and more versatile devices continues to grow. To meet these demands, engineers and designers are increasingly turning to Rigid-Flex PCBs. The circuit boards combine rigid and flexible substrates into a single interconnected structure. This combination allows for complex designs that can bend and flex in specific areas while maintaining rigidity in others. To manufacture rigid flex PCBs, IPC offers advice and best prac......
PCB Stiffeners: An Essential Requirement for Flexible Circuits
A printed circuit board stiffener plays an important role when it comes to offering mechanical support to a PCB. They are particularly helpful for flexible circuit boards, that given their name, are flexible and in need of stiffness in certain places. Stiffeners are particularly required when components are placed in a flex zone & the weight of these components stresses the flex material. These components provide a rigid connection from the flexible portion to the solid board. This solidity makes appl......
The Ultimate Guide to Flexible PCB: Types, Design, and Applications
Key Takeaways JLCPCB 1–4 Layer Flex PCB: Supports 1 to 4-layer FPCs with polyimide (PI) substrates and trace/space down to 3/3 mil. Stiffener Selection: Use PI (0.1–0.25mm) for ZIF connectors, FR4 (0.1–1.6mm) for SMT support, and Stainless Steel (0.1–0.3mm) for high rigidity. Layout Optimization: Use cross-hatched copper ground planes and stagger 2-layer traces to eliminate the "I-Beam effect." Surface & Protection: Combine Immersion Gold (ENIG 1u"/2u") for SMT planarity with flex coverlay to protect ......
Medical Flex Circuits: Manufacturing, Applications, Materials, and Design Guide
Medical flex circuits made to fit inside a 1.0 mm disposable endoscope, wrap around a hearing aid shell, and sit on a patient's arm for ten straight days. When one fails, it is not a warranty return but a device history file and a regulatory conversation. In this guide, you will learn: What separates a medical flex circuit from a consumer one How they are built, tested, and released Polyimide, copper, coverlay, and stiffener choices Fine line, bend radius, and layer count limits What to check before c......