Free Via-in-Pad on 6-20 Layer PCBs with POFV
Free Via-in-Pad on 6-20 Layer PCBs with POFV
For international market, JLCPCB via-in-pad on 6- 20 layer PCBs are upgraded to POFV (Plated Over Filled Via) for free and will continue to be the free default for all upcoming high layer count boards. This means its costs will no longer be added to the total price whether it’s a sample or batch order, allowing everyone to truly enjoy the benefits of JLCPCB’s advanced fabrication. (POFV for 4-layer PCBs still requires charges.)
Via-in-pad has been widely used in high-end PCBs for many years now, but the process has always been a “premium feature” inaccessible to independent designers and hobbyists due to its high cost. Now JLCPCB is going to change this situation with its improved via-in-pad process guaranteeing more stability and reliability than regular tented and plugged vias, using a copper plating thickness of up to 25μm. This improved process is called POFV. It allows flexible, compact routing and makes connections more robust and reliable than with regular vias.
Comparison with JLCPCB Via in Pad(POFV) and Standard Via in Pad
The four pads on the left were made with POFV: the via holes in the pads have been plugged with epoxy and then plated over with copper (“capped”) to create an almost-flat surface. The pad on the right was produced with a regular process and the via hole is exposed; this is undesirable because during reflow soldering the solder can be wicked into the hole, leaving too little on the surface to secure the component.
Outside of pads, the same process is still superior to regular tented/plugged vias, giving a smooth, even appearance and avoiding problems such as insufficiently plugged vias and gas bubbles in the plugging material causing unevenness under BGA components.
1. Benefits of JLCPCB’s POFV Process
POFV technology allows vias to be placed directly within pads. This gives a lot of extra flexibility in routing, especially under BGA components.
Better Electrical Performance
Placing vias directly in pads helps shorten traces and save board space. Whereas regular vias have to keep some distance from the pads they connect to, POFV vias don’t have this limitation. Decoupling components in particular benefit a lot from more direct connections, which in turn means the board runs with more stability.
Protection for the Vias in Harsh Environments
Since vias made with POFV technology are plugged with epoxy and fully plated over, they are protected from corrosion, ensuring reliable operation of the board in moist or warm environments.
2. How They're Made
JLCPCB's high-quality and stable POFV is a combination of plugging and capping. This process creates the following via structure:
As for regular vias, these capped vias are first drilled and then plated; but unlike conventional vias they undergo many extra steps: epoxy filling, heating to dry the epoxy, surface levelling, and then a second plating step to create the cap (surface plating) over the via. Although more complex to produce, their excellent performance and the convenience they bring into the design process are definitely worth the extra steps.
3. POFV Design Requirements
Annular ring: 0.05 mm minimum, 0.075 mm preferred
Via hole size: 0.2 to 0.5 mm
Via hole size | 0.2 | 0.2 | 0.25 | 0.3 | 0.3 (Free) |
Via diameter | 0.3 | 0.35 | 0.4 | 0.4 | 0.45 |
Should be placed more than 0.45 mm from regular PTHs or NPTHs
By making via-in-pad the free default for six layer boards and readily affordable for four-layer boards, JLCPCB aims to continue its mission of providing the most cost-effective service for its customers and making PCB design and prototyping more accessible to everyone.
Recent Posts
• JLCPCB Introduces Discounts for Large PCB Orders
July 25, 2024
• Important Notice: Update on VAT Refund Policy for Orders within China
July 16, 2024
• Flex PCB Now Available at JLCPCB From Special Offer of $2
June 26, 2024
• JLCPCB $4.5/㎡ Off on Quality 4-Layer PCBs
Apr 25, 2024
• JLCPCB's Free Via-in-Pad Process Boosts PCB Design Efficiency by 200%
Apr 17, 2024