This website requires JavaScript.
Coupons
Ship to
Help Center

UL Certification

Last updated on Nov 10, 2026

hdi pcb coupons

What is the Underwriters Laboratory (UL)?

UL is the certifying agency for product safety in the United States of America. The Underwriters Laboratories (UL) test products worldwide according to corresponding U.S. product safety requirements, so that these products may be marketed and sold in every part of the United States of America.

Note

Want to download full compliance reports or other ISO certificates (such as ISO 9001, ISO 14001, RoHS, REACH, etc.)? Click here to explore our complete Certifications Center.

How to add UL marking on the PCB?

JLCPCB's UL identification number is E479892. We currently have 8 active board classes, each with its own UL marking as shown below.

CertificationMaterial TypeBase Material
and Layers
Type Number
JLC-1Nan Ya NP-140F

Nan Ya NP-155F
FR-4 Multi-layer
(4-32 layers)
JLC-2Nan Ya NP-140F FR-4 Single/two-layer
JLC-3
KB-6164-TG135

S1141 TG140

S1000H TG155
FR-4 Single/two-layer
JLC-4
KB-6164 TG135

S1141 TG140

KB-6165 TG155

S1000H TG155

Shengyi S1000-2M - TG170
FR-4 Multi-layer
(4-32 layers)
JLC-5RO4350BRogers
JLC-6ZYF265D(Dk=2.65,Df=0.0019)

ZYF255DA(Dk=2.55,Df=0.0018)
PTFE Teflon
JLC-7ZYF300CA-C(Dk=2.94,Df=0.0016)

ZYF300CA-P(Dk=3.0,Df=0.0018)
PTFE Teflon
JLC-8HY-7000 Aluminum

Currently, the UL marking added by JLCPCB is released online.

When UL marking is required on the PCBs, it is strongly advised that the UL marking is added by JLCPCB to avoid mismatch between selected material and UL type.

"Material Type" must be specified if you require UL marking added by JLCPCB.

In ordering page, three options are available in UL Marking:

①No:

which means JLCPCB will not add UL marking on your behalf. However, you can still add UL marking in the Gerber file by yourself. Please read the precautions below in “Added by Customer”.

②Yes(Any Postion):

which means JLCPCB will add UL marking in a random position on your PCB. When there is no enough space on the board, we may decide not to add the UL marking without prior notice.

③Yes(Specify Position):

which means you could specify the position on the PCB where you prefer JLCPCB add the UL marking. An editor will pop up when you select this option. Besides the position, dimension and rotation of the UL marking are also adjustable.

In the case Any Position or Specify Position is selected, Confirm Production File option is recommended. The silkscreen layer in your original Gerber files must not contain UL markings. Our engineers will add the corresponding UL marking when making the production file based on your order information.

Added by Customer:

Customers can also add the UL marking in the Gerber file by themselves. But please note that when ordering, the base material, board layers, and specified material type selected must match the UL type number in the Gerber file.

Please double check our available UL type as listed on the above chart when you place the order. When there is UL marking already in your gerber file, please DO NOT select Yes(either Any Position or Specify Position) for UL Marking option. UL marking of any other company is not allowed.

Note:

For UL certification compliance, we strongly recommend using the JLC adding UL marking service.

We shall not be liable for any of the below cases:

1. Unauthorized UL marking is added by customer in the original gerber file, causing any further issue/dispute after production.

2. Original gerber file contains UL marking already, which does not match with the selected base material, board layers or specified material type.

3. Original gerber file contains UL marking already, and you select UL marking added by JLCPCB again, resulting repeated UL markings on the board.

4. UL marking added by JLCPCB is required, but there is no space to add on any random position, or elements on PCB prevents UL marking adding on the specified position, resulting no UL marking is printed.