User Guide to the JLCPCB Impedance Calculator
Last updated on Sep 16, 2026

The JLCPCB Impedance Calculator computes track width values and recommended stack-ups from user-input values of board thickness, copper weight, layer, target impedance, conductor spacing (for edge-coupled pairs), and conductor-to-ground gap (coplanar waveguides).
User Interface
1. Layers: Total number of copper layers in the board.
2. Finished Thickness: Thickness of the finished PCB, including soldermask.
3. Internal Copper Thickness: Copper weight for internal layers. The calculator only supports 0.5 oz and 1 oz; for calculations with 2 oz internal copper please contact customer support.
4. External Copper Thickness: Copper weight for the top and bottom layers. Although JLCPCB can produce boards with 2 oz external copper, the calculator only supports 1 oz because (1) the wider tolerance of 2 oz traces hinders impedance control, and (2) most signal traces only carries small currents.
5. Unit: Options are mm, mil, μm, and inch.
6. Impedance (Ω): The desired impedance. The range of accepted values is 20 to 90 Ω for single-ended and 50 to 150 Ω for differential signals.
7. Type: Options are Coplanar Single Ended, Coplanar Differential Pair, Single Ended (Non coplanar), Differential Pair (Non coplanar).Make sure the correct Layer is selected before changing this option.
8. Layer: Which layer the signal should be on.
9. Reference Layer Above: Only needed if the signal is on an internal layer.
10. Reference Layer Below: Does not need to be one layer below the signal; for example for a signal on L3, this option can be L4 or L5. However there must be a ground plane associated with the signal on the reference layer selected.
11. Conductor Spacing: The gap between the two conductors in a differential trace. Increasing conductor spacing increases the calculated trace width.
12. Conductor-to-Ground Gap: The gap between the signal conductor and the surrounding ground in a coplanar waveguide configuration.
Notes
· The first stack-up recommended by the calculator usually has the lowest cost and quickest turn-around.
· The 3313 prepreg replaces the previously available 2313. Their thickness and dielectric constant (εr) are the same.
· For the same nominal copper weight, internal layers have a slightly smaller thickness than external layers due to a small amount of copper being lost in production during deoxidation etc. For example, 0.5 oz copper on internal layers is 15.2 μm thick 4- to 8-layinstead of the nominal 17.5 μm.
· Results for 4- to 8-layer boards are calculated assuming Nan Ya Plastics NP-155F core material, and SYTECH S1000-2M for 10-layer boards and higher. The correct material should be selected when ordering so that the calculated parameters give accurate impedances.
Calculation Parameters Used
| External copper thickness (1 oz) | 1.6 mil |
|---|---|
| Internal copper thickness (0.5 oz) | 0.6 mil |
| Internal copper thickness (1 oz) | 1.2 mil |
| Base soldermask thickness | 1.2 mil |
| Copper-surface soldermask thickness | 0.6 mil |
| Soldermask thickness in between traces | 1.2 mil |
| Soldermask dielectric constant (εr) | 3.8 |
| Trace top width | Trace base width – 0.7 mil |
Nan Ya Plastics NP-155F (4 to 8 layers)
SYTECH (Shengyi) S1000-2M (10+ layers)
The values provided above are for reference only. Some of the values have been calculated from test results by JLCPCB and may be adjusted in the future.