Flex PCB Designing Useful Tips - JLCPCB
5 min
- Considerations for Designing Flex PCBs
Flexible printed circuit boards, or Flex PCBs, are thin, lightweight printed circuit boards that can be bent, folded, and twisted to fit into any shape or size without damaging the electrical connections on the board. Flex PCBs are becoming increasingly popular in various industries, such as aerospace, automotive, medical devices, and consumer electronics. In this article, we will discuss what to consider while designing a Flexible PCB for effective product development.
Currently, flex PCB manufacturing is available on JLCPCB at a special offer of $2 (5 pcs). For new users, there are also up to $60 registered coupons. Just upload your Gerber file and place the order with one click, then wait for your flex PCB designs to be brought into the physical.
Considerations for Designing Flex PCBs
Designing a Flex PCB requires careful consideration of several factors, such as the material selection, circuit layout, and component placement.
The first step in manufacturing Flex PCBs is designing the circuit. Designers use Computer-Aided Design (CAD) software to create a layout that specifies the location of components, traces, vias, and other features on the board, including the PCB Layers stackup which has to be carefully set based on the manufacturer's requirements. Following are some tips to consider while designing a Flex PCB:
- Determine the type of flexible PCB: There are several types of flexible PCBs, including single-sided, double-sided, and multilayer flexible PCBs. It's important to determine the appropriate type of flexible PCB for your application based on factors such as complexity, space limitations, and flexibility requirements.
- Minimize the number of layers: Flex PCBs are typically thinner than rigid PCBs, so it's important to minimize the number of layers to avoid excessive thickness. It's also important to keep in mind that each layer adds complexity and cost to the manufacturing process.
- Allow for sufficient bend radius: Flex PCBs are designed to bend or flex to a certain degree, so it's important to allow for sufficient bend radius to avoid damaging the board. The bend radius should be calculated based on the thickness of the board and the type of material used. Some ECAD tools allow automatic measurement of bend radius based on your design and manufacturer specifications. The thickness of the board is also controlled by the number of design layers and at this level, you can calculate the smallest bend radius based on the PCB layers as follows:
| PCB Layers | Smallest Radius |
|---|---|
| Single side PCB | PCB thickness x 6 |
| Double side PCB | PCB thickness x 12 |
| Multi-layers PCB | PCB thickness x 24 |
When the minimum Bend Radius is not respected, then the produced flex PCB could show compression of the inner flex layer when the board is bend.
- Minimize the use of vias: Vias can add complexity to the manufacturing process and may cause reliability issues. It's important to minimize the use of vias and to use blind or buried vias where possible.
- Use appropriate materials: The choice of materials is critical to the performance of a flexible PCB. Materials such as polyimide and copper are commonly used for flexible PCBs because they are strong, flexible, and have good thermal and electrical properties.
- Place components carefully: Components should be placed on the flexible PCB in a way that allows for flexibility and bending. It's important to avoid placing components in areas that will be subject to excessive stress or strain.
- Use appropriate trace widths and Staggered traces: Trace widths should be chosen carefully to avoid excessive resistance and to allow for sufficient current carrying capacity. Narrower traces can be used on flexible PCBs because the board material is thinner than rigid PCBs, but care should be taken to avoid excessively narrow traces. Avoid drawing stacked traces for double-sided and multi-layer PCBs because such will increase stress resulting in copper circuit thinning at the bend, use staggered traces instead.
- Curved traces and Copper corners: curved traces are necessary for flex PCBs to accommodate the bending and flexing of the circuit without causing stress on the traces. If a trace is too straight or angular, it can crack or break when the PCB flexes. Curved traces allow the PCB to flex smoothly without damaging the trace. Therefore, it is essential to design the curved traces with appropriate radii and spacing to ensure they can withstand the intended flexing and bending.
Copper corners, on the other hand, are necessary to avoid stress concentration on the PCB. When the PCB bends, the corners of the copper traces or pads can experience a significant amount of stress. This can lead to cracking or breaking of the copper, which can result in a failure of the circuit. Copper corners, which are essentially rounded edges, help to distribute the stress evenly across the copper, reducing the likelihood of damage or failure.
- Consider the environment: It's important to consider the operating environment of the flexible PCB when designing it. Factors such as temperature, humidity, and vibration can all affect the performance of the board.
- Component Placement: The placement of components on the Flex PCB should be carefully considered to avoid stress on the board. Components should be placed in areas that are not subjected to bending or twisting.
A good PCB design needs to be made of good materials to achieve the best performance. JLCPCB connects with top raw material suppliers worldwide to provide high-quality true A-grade boards for all kinds of PCB. Meanwhile, JLCPCB has five self-owned intelligent production bases. Due to the large-scale effect on production, JLCPCB is able to minimize production costs and give back profits to our customers as much as possible so that let prices no longer be an obstacle to hardware innovation. Moreover, JLCPCB offers up to $54 registered coupons for every new user. Sign up and upload your Gerber files here and start ordering premium flex PCBs.
Keep Learning
Choosing the Right Bend Radius for Durable Flexible PCBs
Key Takeaways Mastering the bend radius is essential for reliable flexible PCB design. Following IPC-2223 guidelines, maintain a minimum of 6× total thickness for static bends and 100× for dynamic applications, while using thinner RA copper, adhesiveless polyimide, staggered traces, and cross-hatched patterns in flex zones. Proper material selection, layer stackup optimization, and adequate clearance from stiffeners can dramatically extend flex life and prevent premature trace cracking or delamination......
Flex PCB Cost: Complete Pricing Guide & Ways to Reduce Costs
Flex PCB cost is the number that stops most projects cold. You finish a clean polyimide design, upload the Gerbers, and the quote comes back at several times higher than what the same circuit would cost on FR4. Knowing which line items drive that number is what lets you bring it down. In this guide, you will learn: Real flex PCB price ranges for prototypes and production The factors that move an FPC quote the most How does the layer count and quantity change per-board price Why flex costs more than ri......
Flexible Circuit Connector: Types, Features & Selection Guide
A flexible circuit connector clamps onto the bare copper at the end of a flex circuit, so nothing is soldered at that joint. The tail slides into the housing, and an actuator presses a row of spring contacts onto the pads. Every connector is built around one tail thickness. TE's 0.5 mm pitch 2328702 family expects 0.30 mm (12 mil) of flex, because the contact beams are deflected by exactly that dimension. Figure 1: Cross-section of a 0.5 mm pitch FPC connector with the tail inserted Feed it a bare sin......
Polyimide Flex PCB: A Complete Guide for Engineers
A polyimide flex PCB can be folded about 285,000 times when the base film is 25 µm (1 mil) thick. Make that film 75 µm (3 mil), and the same MIT fold test gives up near 6,000 cycles. Bending is a strain problem, not a material problem. Copper sits above the center of the stack, so a bend forces it to stretch around the longer outer path. Figure 1: A polyimide flex circuit folded tight, with a stiffener holding the connector A thicker stack places the copper farther out, resulting in more stretch at th......
Flex PCB Bend Radius: Calculation, Minimum Radius & Design Guidelines
Flex PCB bend radius is the one dimension on an FPC that no design rule check will catch. Bend the circuit tighter than its material allows; the outer copper stretches from its elongation limit, and then it cracks. Figure 1: A flex circuit formed around a mandrel, with bend radius and stack thickness A flex circuit bends around a neutral axis near the middle of its stack. Copper below that line is squeezed, and copper above it is pulled. So the further a layer sits from the line, the harder it is to w......
FPC vs FFC: Understanding the Key Differences Between Flexible Circuit Technologies
The FPC vs FFC decision is really a question about how the copper was made. An FFC consists of flat copper strips laminated between two PET films. Every conductor runs straight from end to end at one fixed pitch, because nothing in that process can make a trace turn or branch. An FPC starts as copper-clad polyimide and is etched exactly like a rigid board. Traces can turn, taper, split onto a second layer, and land under a soldered component. The finished circuit can be as thin as 0.1 mm (4 mil). Figu......