How to Avoid Pitfalls in PCB Design
6 min
- Hole Size in Via Design
- Slot Holes in Via Design
- Hole Attributes in Via Design
- Trace Width and Spacing in Trace Design
- Hatched Copper Filling in Large Area Traces
- Uneven Copper Pour Distribution
- Copper Pour Design
- Conclusion
Designing a printed circuit board (PCB) requires careful attention to various factors to ensure a smooth manufacturing process and avoid potential pitfalls. From hole size and slot design to tra ce width and copper pour considerations, understanding these aspects is crucial for creating reliable and functional PCBs. In this article, we will explore some common pitfalls in PCB design and provide recommendations to overcome them.
Hole Size in Via Design
In PCB manufacturing, a 0.3 mm hole is considered standard, while holes smaller than 0.3 mm are classified as small holes.
Small holes can have several negative impacts on production:
Difficulty in Plating: Smaller holes are more likely to result in unplated or poorly plated holes. For small holes, JLCPCB uses a four-line low resistance process to ensure reliability.
Lower Processing Efficiency: Smaller holes require slower drilling speeds and shorter drill bits. Subsequently fewer boards are drilled at a time. Therefore, when designing, it's advisable to use holes larger than 0.3 mm, considering the use of small holes only when space is limited.
JLCPCB's minimum process capabilities:
Single/double-sided boards: 0.3 mm (inner diameter) / 0.45 mm (outer diameter)
Multilayer boards: 0.15 mm (inner diameter) / 0.25 mm (outer diameter)
Outer diameters should be 0.1 mm larger than the inner diameters, with a recommended difference of 0.15 mm or more.
Slot Holes in Via Design
Short Slots in PCB Drilling: Slots with a length less than twice their width are termed short slots. The optimal length-to-width ratio for short slots is length/width ≥ 2.5 (with a limit of ≥ 2).
Using Hot Air Solder Leveling for Long Slots: For slots selected for hot air solder leveling, it's recommended that one side of the slot hole has a minimum width of 0.4 mm (with an absolute minimum of 0.3 mm) or consider using gold immersion technology.
Hot air solder leveling involves high-pressure and high-temperature processing. Small slot widths can lead to plating peel-off.
Slots with copper plating on one side but no copper ring on the other side, particularly single-sided copper ring slot holes, are more prone to peel-off due to high-temperature stress.
For densely arranged slots, it's advised to use gold immersion technology.
Hole Attributes in Via Design
During design, hole sizes are categorized as VIA holes or PAD component holes, and it's crucial not to mix them.
VIA Holes: These typically serve the purpose of providing electrical connections between circuitry on both sides. During manufacturing, VIA holes are usually treated with soldermask, and JLCPCB does not specify VIA hole size tolerances during production.
PAD Component Holes: These are generally designed as component holes for soldering components.
Mixing them can lead to:
Mistakenly treating VIA holes as PAD component holes and selecting solder mask treatment can result in solder mask covering or clogging component holes, making it unsuitable for soldering. This also makes it difficult to control their size effectively.
Using PAD component holes as VIA holes will prevent the software from giving them soldermask, resulting in vias requiring soldermask treatment remaining uncovered.
Trace Width and Spacing in Trace Design
Thinner traces are not necessarily better; wider traces are preferable whenever conditions allow. Thinner traces have lower conductivity, a higher likelihood of breakage, and lowered yield rates.
Standard trace width and spacing: 4 mils for both. Anything narrower than 4 mils is considered thin.
JLCPCB's minimum trace width/spacing capabilities:
| 1 oz | Single/double-sided: 0.10/0.10 mm (4/4 mil) Multilayer: 0.09/0.09 mm (3.5/3.5 mil); 3 mil allowed in BGA fan-outs PCB coils: 0.254 mm |
| 2 oz | Double-sided: 0.16/0.16 mm (6.5/6.5 mil) Multilayer: 0.16/0.20 mm (6.5/8 mil) |
| 2.5 oz | Double-sided: 0.2/0.2 mm (8/8 mil) |
| 3.5 oz | Double-sided: 0.25/0.25 mm (10/10 mil) |
| 4.5 oz | Double-sided: 0.3/0.3 mm (12/12 mil) |
Hatched Copper Filling in Large Area Traces
When filling large areas with copper, avoid using small hatched grids as this can severely impact production. Choose solid copper fill or large grids instead of small ones. Small grids can lead to several issues:
Inadequate solder mask coverage, as illustrated.
AOI (Automated Optical Inspection) may not detect small grids and may result in errors.
Small grids can cause solder mask peeling, affecting conductivity.
If you must use grid copper filling or need to separate networks, ensure:
Grid line width/spacing is at least 0.254 mm.
There is at least 0.254 mm spacing between traces from the same net.
Uneven Copper Pour Distribution
Uneven Outer Layer Copper Pour: Uneven outer layer copper pouring affects plating current balance and may lead to excessive copper thickness or short circuits due to resin gathering.
Uneven Inner Layer Copper Pour:
In cases where the void area is too large, the resin glue on the PP accumulates and flows toward the copper-free area. This results in thinner boards, copper wrinkling, missing resin causing white spots, and delamination issues.
For products with strict thickness requirements in key areas like gold fingers, if the corresponding inner layer area is too spacious, it can lead to thinning in the gold finger region, poor contact with connector slots, and other problems.
Inconsistent copper coverage area ratios on different layers can also risk board warping.
Copper Pour Design
Avoid Leaving Void Areas: Try to fill copper in void areas whenever possible.
Keep Copper Away from Normal Trace Pads: Ensure that when routing traces, the distance between traces, copper areas, and drill holes is at least 0.5 mm or more. Use solid copper fill rather than small grid copper fill.
Copper pours must be present on all layers where gold finger connectors are located to ensure the thickness of the final board. Care should also be taken to avoid laminate structures with insufficient thickness.
Copper Under Antennas: Follow product design guidelines for copper placement in antenna areas to prevent interference.
Consistent Copper Pour on Both Sides: Ensure that copper is consistently poured on both sides and not left empty on one side.
These design considerations are essential for a smooth PCB manufacturing process and to avoid common pitfalls.
Also Read: Top 6 Custom PCBA Defects Engineers Must Avoid
Conclusion
A well-designed PCB will not only function reliably but also contribute to the overall success of your electronic product. So, take the time to familiarize yourself with these design considerations, incorporate them into your workflow, and enjoy the benefits of a smooth and efficient PCB manufacturing experience.
Keep Learning
GPT-6 Astra PCB Design in KiCad: From Brief to Verified Native Project
Key Takeaways What OpenAI published: The launch page features a 15-second condensed clip of GPT-6 Astra performing PCB layout in KiCad. What the model did: It turned a four-line brief into a 44 × 34 mm, two-layer PCB, covering the circuit, footprints, component placement, routing, and a native two-sheet schematic. Where the work went: Placement and routing were only part of the work. Two linked schematic sheets, project-local libraries, and UUID-based links between 45 components and their footprints w......
GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
Key Takeaways What was tested: GPT-6 Astra was given access to a native EasyEDA Pro 3.2.149 installation and asked to design a stereo TPA3116D2 amplifier from a four-line written brief. What it produced: The run resulted in a 44 × 34 mm, two-layer PCB with 40 SMD components and an editable native EasyEDA Pro project with embedded libraries. Where it failed: The first complete import opened cleanly and looked plausible, yet the initial native verification reported 50 association mismatches involving 12......
AI Tools for PCB Design: Which Tool Fits Your Workflow Stage?
AI tools can now assist with PCB architecture, schematic generation, component selection, placement, routing, and design verification. However, different tools target different stages of the PCB workflow. This guide compares AI tools for PCB design based on what they actually do, what inputs they require, and where they fit within a real engineering workflow. In this guide, you will learn: The 6 types of AI PCB tools and the input each one needs What AI PCB design tools do, compared stage by stage How......
EasyEDA Pro vs KiCad: GPT-6 Astra PCB Design Compared
Key Takeaways What is being compared: Two versions of the same TPA3116D2 stereo amplifier project, each created by GPT-6 Astra in a different EDA tool. The comparison focuses on what you can actually do with the delivered project afterward. Ground copper: In the EasyEDA Pro project, the ground copper is stored as 28 fixed filled regions. In KiCad, it remains as two native copper zones that can automatically refill after layout changes. Verification: KiCad initially reported 46 schematic-parity issues.......
A Practical Guide to ODB Files for PCB Manufacturing
Key Takeaways All-in-One Data: ODB++ combines artwork, netlist, stackup, and drill spans in a single package. Fewer Errors: Embedded netlists allow CAM software to catch errors before production. Pre-Export Checks: Clear DRCs, close the board outline, and verify drill spans in a viewer. Best Practice: Use Gerber for quick quotes and keep ODB++ ready for engineering queries. A Gerber layer might simply say, “draw a 0.5 mm (20 mil) circle here.” ODB++ can describe that same feature as a pad on the VCC n......
AI PCB Design: From Prompt to PCB with EasyEDA Pro
Key Takeaways AI PCB design uses AI agents to automate schematic creation, component selection, layout, and verification inside a real EDA editor — not just generate images. The workflow connects EasyEDA Pro to an AI coding agent (Claude Code or Codex) through the EasyEDA API Gateway, the open-source API Skill, and a local bridge server. Setup takes about ten minutes and is fully local-first: designs, API calls, and intermediate code never leave your machine. Because the agent places real library part......