How to Avoid Shorts and Open Circuits in Dry Film Etching Process
5 min
- Maintaining Adequate Trace Width and Spacing
- Guidelines for Hatched Copper Pours
- Copper Pour Clearances and Design Verification
- Conclusion
- FAQ
When utilizing the dry film etching process, it is crucial to take precautions to prevent short circuits and open circuits in printed circuit boards (PCBs). JLCPCB emphasizes specific considerations to ensure the integrity and functionality of PCB designs. This article provides guidelines for maintaining adequate trace width and spacing as well as utilizing hatched copper pours effectively to avoid defects during the dry film etching process.
Maintaining Adequate Trace Width and Spacing
JLCPCB employs a dry film etching process, which requires careful attention to trace width and spacing. In the case of boards with 2 oz copper, a minimum trace width and spacing of 0.16/0.16 mm must be maintained, as specified in JLCPCB's official PCB manufacturing capabilities. This is essential to avoid the occurrence of shorts and open circuits caused by dry film fragments getting stuck between traces or being washed off thin traces during the etching process. Thicker copper layers (such as 2 oz) are more challenging to etch uniformly than 1 oz copper (which allows 0.10 mm minimum), making these minimum dimensions critical for high-yield production. To ensure reliable connections and prevent circuit discontinuities, any traces in a design that fall short of the specified width and spacing must be adjusted before fabrication.
Guidelines for Hatched Copper Pours
In the dry film etching process, specific focus must be given to hatched copper pours to prevent defects such as open circuits and shorts caused by dry film fragments. When utilizing hatched copper pours, it is crucial to consider the grid line width and spacing. JLCPCB recommends that both the grid line width and spacing should be equal to or greater than 0.254 mm to ensure the desired etching results. This minimum prevents dry film cracking and fragment adhesion, which can also affect subsequent solder mask adhesion.
If hatched copper pours are designed with insufficient width or spacing, it is advisable to either scale up the dimensions or consider making the copper pour solid. These guidelines are vital to mitigate the risk of dry film fragments causing disruptions or unwanted electrical connections during the etching process. For most modern designs, solid copper pours are preferred for superior reliability with dry film technology.
Copper Pour Clearances and Design Verification
Maintaining Proper Clearance in Copper Pours
Moreover, when implementing copper pours—whether hatched or solid—maintaining proper clearance from adjacent traces, pads, and vias is critical to prevent etching residues that could cause shorts. JLCPCB recommends a minimum clearance of 0.2 mm from standard traces and pads, or 0.5 mm for high-speed signal traces, when using solid copper pours. This extra spacing compensates for potential under-etching variations inherent in the dry film process, ensuring clean electrical isolation and reducing the risk of unwanted connections or open circuits in the final PCB.
Utilizing JLCPCB’s Free DFM Checker
To proactively identify and eliminate any violations of these dry film etching rules before submitting files for production, JLCPCB offers a free online DFM (Design for Manufacturability) checker at jlcdfm.com. By uploading your Gerber files, the tool automatically analyzes trace width, spacing, copper pour grid dimensions, and clearances against JLCPCB’s dry film capabilities—such as the 0.16 mm minimum for 2 oz copper and the 0.254 mm recommendation for hatched pours. This instant feedback allows designers to catch potential shorts or open circuits early, significantly improving first-pass yield and avoiding unnecessary fabrication revisions.
Conclusion
By adhering to JLCPCB's instructions and manufacturing capabilities, designers and manufacturers can significantly reduce the likelihood of short circuits and open circuits in PCBs during the dry film etching process. Maintaining adequate trace width and spacing, as well as properly configuring hatched copper pours (or opting for solid pours where possible), ensures the integrity and functionality of the PCB design. These precautions, combined with JLCPCB's advanced dry film technology, contribute to the production of reliable and high-quality PCBs, promoting efficient circuit performance and reducing the need for rework or troubleshooting.
FAQ
Q: What is the minimum trace width and spacing for 2 oz copper boards using JLCPCB’s dry film etching process?
The minimum is 0.16/0.16 mm. Thinner traces risk dry film fragments causing shorts or open circuits.
Q: Why does JLCPCB require a minimum grid line width and spacing of 0.254 mm for hatched copper pours?
Smaller grids can cause dry film cracking and fragments, leading to etching defects and reliability issues.
Q:Should I use solid copper pours instead of hatched ones?
Should I use solid copper pours instead of hatched ones?
Q: What clearance is required between copper pours and adjacent traces, pads, or vias?
Maintain at least 0.2 mm for standard traces/pads or 0.5 mm for high-speed signals to prevent etching residues and shorts.
Q: How can I check my design for dry film etching violations before ordering?
Upload your Gerber files to JLCPCB’s free DFM checker at jlcdfm.com for instant analysis of trace width, spacing, pours, and clearances.
Q: Does the dry film etching process apply the same rules to all copper weights?
No. 1 oz copper allows 0.10 mm minimum, while 2 oz requires 0.16 mm due to thicker copper being harder to etch uniformly.
Keep Learning
Design for Manufacturing and Assembly: A Complete DFMA for PCB Design Guide
Key Takeaways DFMA covers both PCB fabrication and assembly: DFM addresses bare-board fabrication, while DFA addresses component assembly and related process constraints. The biggest decisions happen early: Package choice, layer count, and board outline are usually set well before Gerber export and become expensive to change later. Passing DRC does not guarantee a good footprint: Design rules can verify clearances and copper geometry, but they cannot confirm that a footprint matches the component data......
Get More From Every PCB Panel: Choosing the Right Panel Size
Key Takeaways Panel Drives Cost: Fabs price the whole panel, so maximizing utilization lowers per-board cost. 3 Panel Types: Distinguish raw sheets, fab working panels, and your delivery array. Keep Clearances: Reserve 5 mm process rails and 1–2 mm spacing around V-scores. Match Depaneling Method: Use V-cut (0 mm gap) for rectangles, tab routing for complex shapes. Test Both Orientations: Rotate boards 90° to find the best fit before ordering. PCB panel size is the one number on your order that you ne......
Free DFM Tool: Enhancing PCB Design Efficiency
Design for Manufacturability (DFM) guarantees that the design is best suited for manufacturing and assembly, it is a key process in printed circuit board (PCB) design. Using a Free DFM Tool will improve accuracy and efficiency, by greatly streamlining this process. The advantages of Free DFM Tools, their place in PCB design, and how they could affect your projects are discussed in this article. We will also discuss some typical problems and fixes related to using these tools, highlighting their applic......
Understanding the Importance of DFM Analysis in PCB Design
Design for Manufacturing (DFM) analysis helps you on whether a printed circuit board (PCB) is fit for manufacturing, assembly, and sales. Early in the planning process, it looks for and fixes any possible problems arising throughout production. This will increase manufacturing efficiency and help to save expenses. DFM analysis is quite vital in the complex world of electronics, where even little design errors can create delays costing a lot of money. This article discusses the different types of DFM i......
Thermal Vias in PCB Design for Heat Management
Thermal vias are specialized vias designed to transfer heat from one layer of a PCB to another. These vias are placed near heat-generating components to create a thermal pathway, helping to dissipate heat and reduce the risk of overheating. They are often used with heat sinks, thermal pads, or copper planes to enhance their effectiveness. They are simply plated through holes (PTHs) that are located under a surface-mounted heat source component in a printed circuit board (PCB) that allow heat transfer.......
The Ultimate Guide to PCB Panelization: Tools and Techniques
Printed circuit boards (PCBs) are the backbone of modern electronics. One critical aspect of PCB manufacturing is panelization — the process of arranging multiple PCBs onto a single larger panel for efficient manufacturing and assembly. This technique allows multiple boards to be processed simultaneously, significantly reducing costs and improving production efficiency. In this article, we will provide a comprehensive guide to PCB panelization, covering the tools and techniques required for successful......