Multilayer PCB Design: A Comprehensive Guide
Multilayer PCB Design: A Comprehensive Guide
What is a Multilayer PCB?
A multilayer PCB is a printed circuit board with more than two layers and is comprised of three or more conductive copper foil layers. Multilayer PCBs are standard electrical boards; the top and bottom layers resemble a double-sided PCB but have additional layers on both sides of the core. Multiple layers of double-sided circuit boards are laminated and bonded together with layers of heat-resistant insulation in between. The active and passive components are placed on the top and bottom layers of the multilayer PCB, while the inner stacked layers are used for routing. The inner layers contain vias such as plated through-holes, blind and buried vias, and all electrical connections between them.
These inner stack layers are arranged so that both through-hole (THT) electronic components and Surface Mount Components (SMD) can be soldered on either side of this type of PCB. The application of this technology results in PCBs of various complexities and sizes. Multilayer PCBs can have up to 40 layers.
Why are multilayer PCBs so widely used?
The demand for multilayer printed circuit boards has been on the rise. The push for electronics to be smaller, faster, and more powerful has made multilayer PCBs much more popular. The capability to create multilayer boards opens up a world of possibilities, enabling engineers to build more densely populated circuit boards, facilitating miniaturization. As multilayer PCBs can accommodate more electronic components, they are widely used in modern-day electrical appliances, with variants ranging from 4 to 40 layers.
In a typical four-layer stack-up, to enhance electromagnetic compatibility (EMI) performance, the signal layers should be closely spaced to the ground planes. The close coupling between the signal trace and ground plane typically decreases plane impedance, common-mode radiation, and crosstalk between traces. As the number of layers increases, the PCB board necessitates thin dielectric, resulting in automatic tight coupling between the layers. These stack-ups are commonly utilized in high-speed electronics to provide enhanced EMI performance and signal integrity.
More inner layers will help produce a compact design, lightweight production, durability, and flexibility for a wide range of industries, including consumer electronics, telecommunications, defense, and military. Several applications, such as smart devices, require four to eight layers, while smartphones can use up to twelve.
The Benefits of Multilayer PCBs
Even though the design process for multilayer PCBs is complex and requires domain expertise, they possess several benefits that make them widely used in modern-day advanced electronic devices and electrical appliances. Here are some of the benefits of multilayer printed circuit boards:
Reduced Form Factor: Due to their layered design, multilayer PCBs are more compact than other PCBs with the same functions. Multilayer PCBs offer significant advantages in modern electronics, as smaller, more compact yet more powerful gadgets like smartphones, laptops, tablets, and wearables are leading the new trend.
Lightweight Construction: A smaller PCB weighs less, with multiple laminated layers and electronic components arranged orderly, creating more space for complex electronic applications. Multilayer PCBs are designed to reduce weight and can be utilized in wearable smart devices.
High-Quality: Due to the technological advancements, research, and development invested in creating multilayer PCBs, these types of PCBs typically outperform single and double-sided PCBs in terms of quality. A significant amount of effort is dedicated to the design and manufacturing processes to provide multifunctionality in the compact form factor of the printed circuit board.
More Durable: This printed circuit board is designed to withstand more weight and can also handle the pressure to bind the layers together. Multilayer PCBs provide flexibility to be adjusted according to the applications and do not necessitate a complete redesign.
Less Noisy: RF (Radio Frequency) designs, including antennas, high-speed, and high-frequency signal tracks, require a good grounding shield. A multilayer PCB allows the user to place separate ground and power planes so that RF components can receive a better ground shield, reducing circuit impedance and enhancing the shielding effect.
Better heat dissipation: Due to the high demand for effective heat dissipation in electronic devices, multilayer PCBs can be designed with a metal core heat dissipation layer to fulfill the needs for shielding, heat dissipation, and other distinctive features.
Single Connection Point: Multilayer PCBs are designed to function as a unified unit rather than in conjunction with other PCB components. Consequently, they feature a single connection point instead of the multiple connection points needed when using numerous single-layer PCBs.
Disadvantages of Multilayer PCBs:
Even though there are many benefits of using multilayer PCBs, you should also be aware of the downsides of the manufacturing and designing process. Here is a list of disadvantages of multilayer PCBs:
More expensive: Due to the complexity of the design and manufacturing process, multilayer circuit boards are more costly than single-layer circuit boards. There is an increased amount of labor work and advanced design, along with the pricey assembly machinery.
Complex design process: Multilayer PCBs are more challenging to produce and require additional design time. Designers must adhere to numerous design rules, and manufacturing techniques are more meticulous compared to other PCB types.
Extended lead time: Each board requires significant production time, leading to higher labor costs. Moreover, the production process for multilayer boards is highly intricate.
Required domain expertise: Due to several challenges in the design process, Multilayer PCBs require expertise in CAD tools and an understanding of design rule checks.
Maintenance can be challenging. Repairing a multilayer printed circuit board is difficult if a defect develops. Certain internal layers may not be visible from the exterior, making it more challenging to determine what caused the damage to the component or physical board.
Limited Availability: One of the major challenges with multilayer PCBs is the cost of the equipment required for their production. Not all PCB manufacturers have the financial resources or the demand for this equipment, resulting in limited availability.
Applications of Multilayer PCBs
Due to the advantages of multilayer PCBs over single and double-layer PCBs, they are widely used in high-end electronic equipment where high density, high speed, and high performance are required. Here are some examples of different fields in which multilayer PCBs are used:
Modern-day consumer electronic appliances such as smartphones, wearables, and smart devices utilize multilayer PCBs because of their small form factor and multifunctionality. This feature makes them lightweight and easy to fit into tight spaces.
Telecommunication Industry: Network appliances and transmission devices utilize multilayer PCBs because of their durability and flexibility to adapt to both outdoor and indoor environments. Some common applications include GPS, mobile phone repeaters, and signal transmitters.
Medical devices and the healthcare industry: Medical equipment requires precise functioning for treatment and diagnosis. Multilayer PCBs are used in the medical sector due to their robust functionalities. Multilayer PCBs enhance the performance of electronic applications such as CAT scans, X-rays, heart monitoring equipment, and medical testing devices.
Military and defense: Durability and low weight are essential factors for military and defense use. Multilayer PCBs provide compact designs with small-size boards, allowing more space for other components and custom functionalities. Multilayer PCBs have become integral in military applications such as atomic and nuclear systems that demand high-speed circuits.
Automotive and aerospace systems rely on precision in extreme conditions. Multilayer PCBs can withstand harsh operating conditions without compromising the product's quality and functionality. Examples include car computers, GPS systems, and engine sensors, all of which demand high performance, space optimization, compact size, and heat resistance in PCB boards. Consequently, multilayer PCBs have become the preferred choice for designers in these industries.
Multilayer PCBs are also utilized in various industries with specific space and speed requirements, such as securities, IoT (Internet of Things), and home appliances. They are used in a wide range of applications, from weather analysis equipment to atomic accelerators, fiber optic sensors, and alarm systems.
How are the layers stacked in a single, double, and multilayer PCB?
In a single-layer PCB, all components are mounted on one side of the board. In a double-layer PCB, components are mounted on both sides of the board. In a multilayer PCB, multiple layers of conductive material are sandwiched between insulating layers, allowing for more complex circuits and higher component density.
Ordinary PCBs are divided into single-sided and double-sided alignment, commonly known as single-sided and double-sided boards. They typically have one or two copper conductive layers in the design. However, high-end electronic products may have multiple layers of copper lines stacked in the core due to space design constraints. Each layer of lines is produced, positioned, and pressed together sequentially using optical equipment. This process allows for the stacking of numerous circuit layers on a single board, creating a multilayer circuit board. A multilayer circuit board is defined as any circuit board with two or more layers. Multilayer PCBs are categorized as rigid PCBs, flexible PCBs, and rigid-flex PCBs.
How can you distinguish between single-layer and multilayer PCBs?
To identify the PCB type, two basic procedures can be followed as mentioned below:
1. Hold the PCB in a cross-sectional view with a light source; if the inner core is opaque or entirely black, it indicates a multilayer board. If the core is transparent, it is a single or double-sided board. Single-sided boards are easy to identify because they do not have copper inside the holes.
2. A single-layer PCB has only one layer of lines (copper layer), without metallization in the holes, and no plating procedure. In contrast, a double-layer PCB consists of two lines (copper layer), with both metalized and non-metalized holes, along with a plating procedure.
Multilayer PCB Laminate Technology
Multilayer PCB (Printed Circuit Board) laminate technology is a critical advancement in electronic circuit design, enabling the creation of more complex and compact devices. In a multilayer PCB, multiple layers of conductive copper and insulating materials, referred to as laminates, are stacked and bonded. This structure facilitates intricate circuitry and high component density by offering multiple paths for electrical connections, reducing the reliance on external wiring, and enhancing signal integrity. The laminates consist of prepreg (pre-impregnated with resin) and core materials, meticulously chosen for their electrical, thermal, and mechanical properties.
These materials must be precisely aligned and bonded to form a cohesive and reliable multilayer stack. Advanced manufacturing processes, including drilling, plating, and etching, create vias and interconnections between layers. This technology supports the growing demand for smaller, faster, and more efficient electronic devices, finding applications in various industries, including telecommunications, automotive, aerospace, and consumer electronics. As technology advances, multilayer PCBs continue to evolve, incorporating innovative materials and techniques to enhance performance and functionality.
JLCPCB Multilayer PCB: High precision and Professional PCB
JLCPCB :$2 for Multilayer PCB
Unleash the full potential of your electronic designs with JLCPCB's high-quality multilayer PCB manufacturing services. We deliver precision, reliability, and innovation for your most complex projects. Our advanced fabrication technology ensures superior performance and durability, catering to various applications from consumer electronics to industrial systems. With competitive pricing, fast turnaround times, and exceptional customer support, JLCPCB stands as your trusted partner in bringing your intricate PCB designs to life.
JLCPCB is a custom one-stop shop for PCB solutions, serving engineers worldwide in PCB manufacturing and assembly services. Our team will guide you through the process of producing your multilayer PCB. With our experienced team having created thousands of multilayer PCBs, ranging from simple 2-layer to complex 20-layer PCBs, we offer top-quality A-grade materials, state-of-the-art equipment, instant online quotes, 24-hour quick turnaround, fast delivery, and the most competitive prices in the market.
Recent Posts
• Multilayer PCB Design: A Comprehensive Guide
July 27, 2024
• Future Trends and Innovations in Flex PCB Technology
July 26, 2024
• Exploring Electronic Sensors: The Backbone of Modern Technology
July 22, 2024
• Understanding and Utilizing Breakout Boards in Electronics Projects.
June 29, 2024
• Comparing HASL and ENIG Surface Finishes for PCBs
June 29, 2024