Free 3D printing prototype with X Resin
Free 3D printing prototype with X Resin
X Resin Free Sample Participation Rules:
-1.The volume of printed parts must not exceed 150 cm³;
-2.The number of prints must not exceed 2 pieces;
-3.Each individual is limited to participating in the free sample offer only once;
-4.Each order must pay a minimum of $1 USD, as export standards dictate that the value of goods cannot be zero. Therefore, even if the order consists solely of free printed X resin items, a payment of $1 USD is required;
-5.The Free Coupon is only valid for certain regions/ countries,
About X Resin:
X Resin is a novel resin introduced by JLC3DP, employing the concept of blind box resin, utilizing a randomized distribution for resin printing. There is a high probability of randomly matching high-value resin materials such as Imagine Black and 8001, with prices starting as low as $0.04/g. Orders are shipped within 72 hours, promising an experience filled with anticipation and the unknown.
Note:All of the following resin materials participate in the X Resin Free Prototyping Activity.
Suitable Customer Base for X Resin:
X Resin is highly suitable for makers, engineers, individual enthusiasts, and similar groups for project validation and preliminary sampling. Moreover, there are no minimum order requirements.
Points to Note:
- Due to the unique resin allocation mechanism of X Resin, orders will be printed on different devices with varying parameters. Therefore, only sample orders are supported, not bulk orders.
- X Resin is ideal for sample validation, collectible figurines, and personal DIY projects. It is not suitable for mass production or parts requiring specific performance and precision. It is recommended to choose dedicated materials for such purposes.
- An order may be assigned to multiple devices for printing, resulting in potential variations in color and precision. This is considered normal, and such claims for after-sales support will not be entertained.
Note: JLC3DP reserves the right to interpret the rules of this promotion.
Zuletzt aktualisiert am Mar 18, 2024