3D Printing Special Charges Cases
For 3D printing, all the prices are based on the online calculator. Price is subject to additional charges for the below situation.
1. Special-shaped models with many thin support structures or hollow structures, $8 extra are required as more processes and more time are needed for manufacturing.
2. For large volume model with 250mm + length(like below), an extra cost of $8 is required and build time will add one more day.
For large volume model with 500mm + length(like below), an extra cost of $16 is required and build time will add one more day.
Last updated on Oct 27, 2022
Was this article helpful?
Yes
No