This website requires JavaScript.

CNC Machining - JLCPCB Q&A

Sheet Metal - Countersunk Holes

Hello! When I upload a STEP file to the sheet metal calculator, are countersunk holes automatically taken into account for......

1 Reply Asked by 65*******2A
Aluminum 5052 sheet metal surface finish

Hi, is it possible to do a brushed+anodizing+silkscreen finisch on aluminum 5052 sheet metal parts?

2 Replies Asked by 44*******5A
DXF file for laser engraving

Generating a DXF file for the laser engraving results in only outlines of the graphic I would like engraved on the surface......

1 Reply Asked by 21*******4A
Subject: Question about Surface Finish on Aluminum 6061

Dear JLCCNC Team, I would like to ask about the bead blasting + anodizing surface treatment on Aluminum 6061. Could you pl......

1 Reply Asked by 96*******8A
Silk Screen Ordering

What information is needed to order Silk Screening on a part? Does the DXF need to include just the image/text to be print......

1 Reply Asked by 57*******9A
Hardcoat anodizing black

I want to create a frontpanel in Aluminum 6062 Hardcoat anodizing black. As the fonts should be visible they should be pro......

1 Reply Asked by 83*******5A
small via size?

via pad 0.4pi, drill 0.15pi is it possible?

3 Replies Asked by 80*******8A
Sheet Metal Cutting & Bending

Do you have sheet metal cutting & bending services? or is it just CNC machining services?

1 Reply Asked by 26*******8A
What is the minimum hole diameter you can CNC make in aluminum ?

Hello, what is the minimum hole diameter you can CNC make in aluminum ?

1 Reply Asked by 44*******5A
Machining size

What are the maximum and minimum machining sizes for CNC ?

1 Reply Asked by 38*******7A
What is the thickness of your different anodizing coating ?

Hi, what is the thickness of your different anodizing coating ?

1 Reply Asked by 35*******9A
Hi, is it possible to tap the small holes in the CNC machined part with M3 threads?

Hi, is it possible to tap the small holes in the CNC machined part with M3 threads?

1 Reply Asked by 44*******5A