Protective Measures for PCBs: Safeguarding Electronics from Environmental Factors and Electrical Hazards
Protective Measures for PCBs: Safeguarding Electronics from Environmental Factors and Electrical Hazards
Printed Circuit Boards (PCB’s) serve as crucial parts of electronic devices providing the framework for connecting various electrical components. Put in place strong protection measures to guarantee the dependable and durable operation of PCBs. PCB protection means preventing external influences, electrical problems, mechanical stress, and excessive temperatures from harming the board and it’s components.
In the subsequent sections, we will delve into nine methods, which are summarized into five major areas. Let's explore the world of PCB protection and discover how to safeguard your PCB’s against the challenges they may face in their operational environment.
Environmental Protection:
One crucial component of PCB protection is environmental protection. We often subject PCBs to a variety of environmental conditions, including moisture, dust, chemicals, and temperature fluctuations. These behaviors might lead to corrosion, short circuits, component failure, and degraded performance.
Conformal Coating: Conformal coating is a thin protective layer put on the surface of the PCB. It blocks fluctuations in temperature, chemicals, dust, and moisture. Acrylics, silicone, urethane, and epoxy are some examples of common conformal coating materials. Using techniques like spray coating, dip coating, or brush coating, we apply the coating to the PCB, following its curves to cover the solder connections, components, and traces.
Encapsulation: Encapsulation refers to entirely covering the PCB with a protective layer, or to simply a few selected components having a protective layer. To form a robust and long-lasting barrier, protective material is poured or injected around the PCB or component. Encapsulation improves mechanical strength, electrical insulation, and shock and vibration resistance. As a result, the PCB receives protection from physical harm, chemicals, moisture, and dust.
Varnish/Dipping: Protection against moisture, corrosion and a certain degree of mechanical stress is achieved by dipping or coating the PCB with a varnish or protective solution to provide a protective layer. Because the PCB is immersed or coated in a varnish or protective solution, we form a thin layer on the surface of the circuit board. This technology is more typically employed in applications where a more cost-effective way of protection is required.
Environmental Sealing: Sealing methods such as gaskets, O-rings, or watertight housings can provide a barrier against external pollutants when we need to protect a PCB from water, dust, or other environmental variables. In addition, we will put the seals around ports, connectors, and other holes in order to keep moisture and dust out of PCBs and enclosures.
Electrical Protection:
Over-current and Over-voltage Protection: We might use circuit breakers, varistors, and transient voltage suppressors (TVS diodes) to protect of PCBs from over-current and over-voltage situations. These gadgets aid in preventing harm from spikes in voltage or high current.
Grounding: Grounding entails creating a reference point or common ground potential for all components and circuitry on the PCB. It lessens the chance of EMI and minimizes voltage variations. In practice, we can connect all ground terminals of components and subsystems to a single common ground point on the PCB. This behavior reduces ground loops and ensures a consistent reference potential. Or, in mixed-signal PCBs, separate analog and digital ground planes to prevent noise coupling between sensitive analog components and noisy digital circuitry. We can use separate Vias for connection.
Shielding: Shielding is using conductive materials to form barriers around sensitive components or circuits. The purpose of that is aiming to block external EMI. To achieve this, we could use metal cans or boxes to confine electromagnetic radiation around sensitive components like oscillators or high-frequency circuits. For efficient shielding, connect the shield container to the ground plane.
ESD Protection: Electrostatic discharge (ESD) protection measures such as ESD diodes, grounding, and proper handling procedures are implemented to safeguard the PCB from ESD events. By applying appropriate grounding and shielding procedures, we may reduce radio frequency interference (RFI) and electromagnetic interference (EMI). When using this method, we need to pay attention to the proper placement and routing of ground traces, the use of ground planes, and the use of shielding techniques (such as conductive enclosures or shielding materials) to prevent unwanted electrical noise and interference.
There are 15 types of ESD gadgets in JLCPCB to help you protect device:
At JLCPCB, we offer a range of circuit protection devices
Thermal Management:
Excessive heat can adversely affect PCB components and their performance. Overheating can lead to component failure, thermal runaway, and reduced service life. Adequate thermal management, including the use of heat sinks, fans, and proper ventilation. Additionally, incorporate thermal Vias into the PCB design. Vias provide a path for heat to flow from a component to a larger ground plane or heat sink. Use copper pours or large-area copper connections to thermal Vias to enhance heat dissipation. The copper area acts as a heat sink, helping to distribute heat to the PCB surface and improve thermal conductivity. Not only that, choose PCB materials with high thermal conductivity, such as metal-core PCBs or PCBs with thermally conductive dielectric layers. These materials facilitate efficient heat transfer and help dissipate heat from Vias and components more effectively.
Mechanical Protection:
Mechanical stress on PCBs can arise from bending, vibration, and shock. This stress can cause solder joint failures or disconnected components. Stiffeners and support structures are examples of mechanical reinforcement techniques that help reduce the effects of mechanical stress and improve the PCB's overall longevity.
Specifically, when installing the PCB, we can use the proper mounting approaches, such as screws, standoffs, or snap-fit connections. By providing a robust and secure mounting, these strategies lessen the chance of PCB bending and the strain on the Vias. Additionally, we may strengthen PCB key spots such as those close to Vias or vulnerable to mechanical stress. To improve the mechanical strength and stability of the PCB, we would add more copper traces, strengthen with epoxy or glue, or employ methods like layers of carbon fiber or fiberglass. Besides that, we can use shock-absorbing materials like foam or rubber gaskets between the PCB and the mounting surface. Because these materials absorb and attenuate shock and vibration, they reduce stress on Vias and other components.
PCB Layout Design:
The design of the PCB layout is of the utmost importance to provide the PCB with efficient protection.
As we previously discussed, proper PCB layout design practices may help lower electromagnetic interference (EMI) and increase overall PCB reliability and protection. These practices include trace routing, ground planes, signal integrity concerns, and the separation of high- and low-power components. By avoiding routing sensitive traces or components close to high-voltage networks, we reduce the chance of damage from high-voltage spikes. In the early PCB design process, you must decide on the pads' and holes' sizes. Finding the ideal ratio of pad to hole size becomes more crucial as both pad and hole sizes shrink. In particular, while utilizing through holes. One further crucial factor to consider is the PCB pads' form. Depending on the manufacturing process, the PCB footprint may change. For instance, we usually need a greater floor area for wave soldering than for infrared re-flow soldering.
Conclusion
Through comprehension and application of these PCB protection techniques, you may reduce the possibility of malfunctions, lengthen the lifespan of your PCBs, and augment the general dependability of your electronic apparatuses. To guarantee outstanding performance and safeguard your investment, you must be knowledgeable about and apply PCB protection techniques.
Recent Posts
• Rigid PCB vs. Flexible PCB: Making the Right Choice
June 14, 2024
• Flex PCB Designing Useful Tips - JLCPCB
June 14, 2024
• Introduction to 6-Layer PCBs: Structure, Design, and Applications
June 4, 2024
• Comparing 6-Layer PCBs with Other Multilayer PCBs: Cost, Complexity, and Optimization
June 3, 2024
• Advantages of 6-Layer PCBs: Performance, Reliability, and Design Flexibility
June 3, 2024